Element Records

Element records store information about the elements used in scenarios. This topic provides an alphabetical list and description of the fields that exist for the Element family. The information in the table reflects the baseline state and behavior of these fields.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.

Field

Data Type

Description

Behavior and Usage

Is Primary? Logical Indicates whether or not the associated record is the "Primary" Scenario element. This field is required.
Name Character The name of the element record. This field is required.
Planned Life End Numeric The amount of units at the end of operation. This field is only available for Fleet Management analyses. This field is required.
Planned Life Start Numeric The amount of units at the beginning of operation. This field is only available for Fleet Management analyses. This field is required.
Quantity Numeric The quantity of the element record. This field is required.
Scenario Key Numeric The Entity Key associated with the scenario record. System Generated field that is hidden by default.

Copyright © 2018 General Electric Company. All rights reserved.