Cost records store information about the cost data used in LCC. This topic provides an alphabetical list and description of the fields that exist for the Cost family and appear on the LCC Cost datasheet. The information in the table reflects the baseline state and behavior of these fields.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Field |
Data Type |
Description |
Behavior and Usage |
---|---|---|---|
Cost Name | Character | The name of the cost. | Text is entered in the Cost Name field. |
Cost Type | Character | Determines the type of cost for the record. |
The value in this field can be:
|
Element Key | Numeric | The Entity Key of the element record. | System Generated field that is hidden by default. |
Is Primary | Logical | Indicates whether or not the cost is for the primary element. | This field is required. |
Resource Name | Character | The name of the resource. | Text is entered in the Resource Name field to describe the resource. |
Scenario Key | Numeric | The Entity Key of the scenario record. | System Generated field that is hidden by default. |
Total | Numeric | The total of costs of the cost record. | This field is the sum of the costs of all periods associated with this cost. |
Copyright © 2018 General Electric Company. All rights reserved.