Analysis records store information about the fields in the Analysis family that are used to populate the fields for the Analysis Definition. This topic provides an alphabetical list and description of the fields that exist for the Analysis family and appear on the LCC Analysis datasheet. The information in the table reflects the baseline state and behavior of these fields.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Field |
Data Type |
Description |
Behavior and Usage |
---|---|---|---|
Analysis Period Unit | Character | The time for unit period. |
The default value for this field is years. This field is required. |
Annual Effective Interest Rate | Numeric | The annualized compounding interest rate. |
This value must be a positive number. This field is required. |
Annual Escalation Rate | Numeric | The current price or value minus the initial cost or value in a one year period, divided by the initial price. |
This value must be a positive number. This field is required. |
Annual Nominal Interest Rate | Numeric | The stated interest rate of a given loan. |
This value must be a positive number. This field is required. |
Assumptions | Text | User entered field describing any/all relevant Assumptions. | Text is entered in the Assumptions field. |
Constraints | Text | User entered field describing any/all Constraints. | Text is entered in the Constraints field. |
Currency | Character | The currency used by your organization. | The default value for this field is US Dollars. |
Declining Balance Factor | Numeric | The factor that determines accelerated depreciation in which the amount of depreciation that is charged to an asset declines over time. |
The default value for this field is 2, which represents double declining balance depreciation. The value in this field must be a positive number. |
Dependencies | Text | User entered field that described any/all dependencies. | Text is entered in the Dependencies field. |
Depreciation Method | Character | The method used to determine depreciation of the asset over time. |
The value in this field can be:
This field is required. |
Description | Text | User entered field that described any/all descriptions. | Text is entered in the Description field. |
End Date | Date | The date on which the analysis ended. |
This field is calculated by adding the analysis period to the start date. This field is required. |
Is Fleet Management | Boolean | Identifies whether or not the analysis is used for fleet management. | This field is calculated by your selection when creating a new analysis. |
Interest Rate Type | Character | The type of interest rate, either Simple or Compound, used for the analysis. | This field is required. |
Name |
Character | The name of the analysis. | This field is required. |
Number of Periods | Numeric | The number of periods (for example, years) which the analysis covers. |
This field is required. |
Objectives | Text | The objectives for the analysis as defined by your organization. | Text is entered in the Objectives field. |
Start Date | Date | The date on which the analysis began. |
You can use the Calendar feature to select the date on which the analysis began. This field is required. |
Tax Rate | Numeric | The tax rate associated with the analysis. |
This value must be a positive number. This field is required. |
Copyright © 2018 General Electric Company. All rights reserved.