Create a Secondary Element in the Cost Data Grid

Steps

  1. Access a Cost Data grid.
  2. In the primary element cell, select .

    The Add Secondary Element window appears.

  3. If you want to add an element that is listed in the hierarchy:

    1. Beside the Asset Hierarchy ID box, select .

      The Hierarchy window appears.

    2. Navigate to and select an Asset, and then select Done.

    3. Enter values in the Secondary Element and Quantity boxes.

      Note: Quantity, which has a default of 1, is used as a multiplier. For example, if the quantity is equal to 10, all of the operating and capital costs are multiplied by 10.

    4. On the Add Secondary Element window, select OK.

    -or-

    If you want to add an element that is not listed in the hierarchy:

    1. Enter values in the Secondary Element and Quantity boxes, and then select OK.

      IMPORTANT: When adding an asset not listed in the hierarchy, the import features may not have the context needed to function and will return null results.

    The secondary element appears in the Cost Data grid.

Copyright © 2018 General Electric Company. All rights reserved.