Safety Integrity Level records are used to determine the SIL value and contain the boundary values for the required probability of failures for different safety integrity levels. This topic provides an alphabetical list and description of the fields that exist for the Safety Integrity Level family. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.
This family is not enabled for site filtering, which means that records in this family can be accessed by any user with the appropriate license and family privileges. See the Site Filtering section of the documentation for more information.
Field |
Data Type |
Description |
Behavior and Usage |
---|---|---|---|
Lower Bound | Numeric | The lower boundary value for the Safety Integrity Level. | You can enter a value manually. |
Mode of Operation | Character | Indicates whether the record defines the SIL value for a safety system operating on low demand mode or on continuous mode. | You can enter a value manually. |
Safety Integrity Level | Numeric | The SIL value for which the boundary values are defined in the record. | You can enter a value manually. |
Upper Bound | Numeric | The upper boundary value for the Safety Integrity Level. | You can enter a value manually. |
Copyright © 2018 General Electric Company. All rights reserved.