Consequence Modifier Records

Consequence Modifier records store details about conditional modifiers (i.e., an event or action that can increase or decrease the probability that a risk may occur if not mitigated). This topic provides an alphabetical list and description of the fields that exist for the Consequence Modifier family and appear on the Conditional Modifier datasheet. The information in the table reflects the baseline state and behavior of these fields.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.

Field

Data Type

Description

Behavior and Usage

Conditional Modifier ID

Character

The identification for the conditional modifier.

The value entered in this field must be unique.

This field is required.

Description

Character

The description of the conditional modifier.

You can enter a value manually.
Modifier Type Character The type of conditional modifier.

This field is required. This field is labeled Type on the Consequence Modifier datasheet.

This field is populated with the value in the Modifier ID field of Consequence Adjustment Probabilities records.

Probability Numeric The probability that the conditional modifier can occur.

This field is disabled on the datasheet.

Based on your selection in the Type field on the Consequence Modifier datasheet, this field is populated with the value in the Default Value field in the Consequence Adjustment Probability record.

This value is multiplied by the value in the Enabling Event/Condition Probability field on the Layer of Protection Analysis (LOPA) datasheet to calculate the final probability for the initiating event.

Copyright © 2018 General Electric Company. All rights reserved.