LOPA is used for quantitative assessment of the probability of occurrence of an incident or risk and for assessing the SIL value. With GE Digital APM, you can use the values calculated in LOPA to quantitatively assess the SIL and derive a qualitative risk rank mapping for an Instrumented Function in SIS Management. You can then create recommendations that can be promoted to Asset Strategy Management (ASM).
GE Digital APM maps the quantitative values calculated using LOPA with the Risk Matrix configured for the site to which the LOPA belongs, and then assigns the unmitigated risk in the Risk Matrix. The following values in the LOPA are used to derive at the unmitigated risk rank:
Unmitigated Consequence Frequency: The value in the Unmitigated Consequence Frequency field is mapped to the Probability value in the Risk Matrix in one of the following ways:
Note: GE Digital APM assumes that you have created the Risk Matrix for your site using probability values that have been standardized to be measured in terms of years.
Based on the Probability and Consequence values, GE Digital APM identifies the unmitigated risk rank associated with the selected Risk Category. A Risk Assessment record, which stores details such as the driving risk category and the unmitigated risk rank value, is created and linked to the LOPA.
If you assess the SIL value for an Instrumented Function using a LOPA that is linked to a Risk Assessment, and then create a recommendation for the Instrumented Function, the Mitigated Risk section appears in the Recommendation. In the Mitigated Risk section, the following details appear:
On the Risk Matrix, in the Risk Category that you selected in the LOPA, the icon appears on the cell corresponding to the unmitigated risk rank. You can then select the mitigated risk rank for the category.
Suppose that you have configured a Risk Matrix for Site X with the following values in Risk Probability records for the Risk Category Operations:
Risk Probability Name | Probability | Failure Interval | Failure Interval Units |
---|---|---|---|
Frequent | 1 | 1 | years |
Probable | 0.1 | 10 | years |
Possible | 0.01 | 100 | years |
Remote | 0.001 | 1000 | years |
Improbable | 0.0001 | 10000 | years |
In Site X, suppose that you created a LOPA with the following details:
For the above example, the probability value in the Risk Matrix that is less than the unmitigated consequence frequency is 0.001. Therefore, on the Risk Matrix, the unmitigated risk will be mapped to the cell corresponding to Probability value 0.001 and Consequence value High.
Suppose that you have configured a Risk Matrix for Site X with the following values in Risk Probability records for the Risk Category Operations:
Risk Probability Name | Probability | Failure Interval | Failure Interval Units |
---|---|---|---|
Frequent | 5 | .2 | years |
Probable | 1 | 1 | years |
Possible | 0.3 | 3.33 | years |
Remote | 0.1 | 10 | years |
Improbable | 0.05 | 20 | years |
In Site X, suppose that you created a LOPA with the following details:
For the above example, the unmitigated consequence frequency is lower than the lowest probability value (i.e., 0.05) in the Risk Matrix. Therefore, on the Risk Matrix, the unmitigated risk will be mapped to the cell corresponding to Probability value 0.05 and Consequence value Medium.
Related Information
Copyright © 2018 General Electric Company. All rights reserved.