Install Redis - High Availability Configuration

GE Digital APM Servers are set up either using a medium cache configuration or a high availability configuration.

Steps

Note: By Default, GE Digital APM Installer performs these steps automatically for a standard install.
  1. On the GE Digital APM Server machine, login as an administrator.
  2. Open a command prompt window.

  3. In the command prompt window, change to the directory where the file was copied.
  4. Enter the following command in the window: redis-server --service-install redis.windows.conf

  5. Press Enter on the keyboard.

    Redis is installed as a service.

  6. On the Windows Start menu, enter Services.msc in the search box.
  7. Press Enter on the keyboard.

    The Services window appears.

  8. Double-click on Redis service.

    The Redis service is now running on the GE Digital APM Server machine.

Copyright © 2018 General Electric Company. All rights reserved.