The table below provides an alphabetical list and description of the fields that exist for the Inspection Taxonomy Configuration family. The information in the table reflects the baseline state and behavior of these fields.
This family is not enabled for site filtering, which means that records in this family can be accessed by any user with the appropriate license and family privileges. See the Site Filtering section of the documentation for more information.
Field |
Data Type |
Description |
Behavior and Usage |
---|---|---|---|
Checklist Template | Character | Stores and displays the defined Checklist Configuration Template name. | This field is populated automatically by the GE Digital APM system with the name of a Checklist Configuration Template that has been linked to a Taxonomy Configuration. |
Checklist Template Key | Number | Stores the entity key of the defined Checklist Configuration Template. |
This field is populated automatically by the GE Digital APM system. IMPORTANT: Do not modify the contents of this field. |
Inspection Family | Character | Stores the defined Family ID and caption. | This field is populated automatically by the GE Digital APM system with the Family ID and caption of an Inspection Family that has been linked to a Taxonomy Configuration. |
Taxonomy Category | Character | Stores the defined Taxonomy Category. | This field contains a list of available Taxonomy Categories that are available in [GE Digital APM. This field can be modified in the Taxonomy Configurations section of Application Settings. |
Taxonomy Class | Character | Stores the defined Taxonomy Class. | This field contains a list of available Taxonomy Classes that are available in [GE Digital APM. This field can be modified in the Taxonomy Configurations section of Application Settings. This field is filtered based on the selected Taxonomy Category. |
Taxonomy Type | Character | Stores the defined Taxonomy Type. | This field contains a list of available Taxonomy Types that are available in [GE Digital APM. This field can be modified in the Taxonomy Configurations section of Application Settings. This field is filtered based on the selected Taxonomy Category and Taxonomy Class. |
Copyright © 2018 General Electric Company. All rights reserved.