Inspection Profile

Inspection Profiles represent subcomponents of a piece of equipment on which inspections are performed. The following table provides an alphabetical list and description of the fields that exist in the Inspection Profile family. By default, all fields in the Inspection Profile family appear on the Inspection Profile datasheet.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.

Field Data Type Description Behavior and Usage

Item Category

Character

The type of subcomponent (e.g., pipes) that exists on the piece of equipment needing inspection.

This field appears as a list that contains the System Code IDs and Descriptions in the MI INSPECTION PROFILE CATEGORY (Inspection, Profile Category) System Code Table. The Profile Configuration setting determines how this field will be populated. You can modify the value in this field using the datasheet.

Item Description

Character

A description of the subcomponent.

You can specify a value for this field using the datasheet.

Item ID

Character

The ID of the subcomponent.

This field is populated automatically based on the value in the Item Category field. You can modify the value in the Item ID field using the datasheet.

RBI Component

Character

The Record ID of the RBI Component that is associated with the Inspection Profile.

This field appears as a list that contains the Record IDs of all RBI Components that are linked to the associated Equipment. This field is null, by default.

This field is enabled only when the Risk Based Inspection license is active.

RBI Component Family

Character

The RBI Component subfamily that is associated with the Inspection Profile.

This field appears as a list that contains the captions of all RBI Components subfamilies that exist in the baseline GE Digital APM database. This field is populated automatically when you select a value in the RBI Component list. You can modify the selection in this list using the datasheet.

Sequence

Numeric

The order in which the subcomponent should be inspected, relative to other subcomponents on the piece of equipment.

You can specify a value for this field using the datasheet.

Copyright © 2018 General Electric Company. All rights reserved.