The Inspection Finding Checklist represents subcomponents belonging to the item that you are inspecting. Since the subcomponents that you will need to inspect will differ based on the type of inspection that you are performing, the items that appear in the Inspection Finding Checklist will differ based on the Inspection subfamily.
The baseline Inspection families are:
Each of these families is hard-coded to use a particular System Code Table to create the finding sections and rows that appear in the grid on the Inspection Findings Checklist page. The sections and rows on the Inspection Findings Checklist page are built from System Code Tables and referenced System Codes.
Note: The Checklist Inspection Template family is not hard-coded to include specific Checklist Findings. The Checklist Findings are defined by the checklist categories and items for the Checklist Configuration Template.
The baseline GE Digital APM database contains the following System Code Table:
This System Code Table contains the following System Codes:
Each of the System Codes that belong to this System Code Table contain referenced System Codes. For example, the System Code Supports contains the following referenced System Codes:
Together, the System Code Tables, System Codes, and referenced System Codes determine which sections and rows you will see on the Inspection Finding Checklist page. Using this example:
Each field within the checklist can be modified by the user to best fit the work process.
Copyright © 2018 General Electric Company. All rights reserved.