GE Enterprise records represent the Enterprises imported from GE System 1 or GE SmartSignal. These records must be configured correctly in order to import GE Tag records.
This topic provides an alphabetical list and description of the fields that exist for the GE Connection family and appear on the GE Enterprise datasheet. The information in the table reflects the baseline state and behavior of these fields.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Field |
Data Type |
Description |
Behavior and Usage |
---|---|---|---|
Active |
Logical |
Indicates whether the system is active. |
Selecting this check box indicates that the Enterprise is active. |
Enable Integration |
Logical |
Indicates whether the system is enabled. |
Selecting this check box enables the automatic import of GE Tags belonging to the corresponding Enterprise in GE Digital APM database. |
Minimum Severity |
Number |
Minimum severity of Events to be imported. |
Only Events with the selected Severity or higher will be imported in GE Digital APM database. The default value in this field is Info (0). Note: Minimum Severity filtering does not apply to start up and shutdown Events, as these always have a Severity of Info (0). |
The following fields in GE Enterprise records are read-only and are populated automatically by the GE Service:
Note: Refer to GE System 1 or GE SmartSignal documentation for more information on these fields.
Copyright © 2018 General Electric Company. All rights reserved.