GE Connection records establish the connection to the GE Fleet message broker. To establish the connection to the message broker, certain fields on the GE Connection record must be completed.
This topic provides an alphabetical list and description of the fields that exist for the GE Connection family and appear on the GE Connection datasheet. The information in the table reflects the baseline state and behavior of these fields.
This family is not enabled for site filtering, which means that records in this family can be accessed by any user with the appropriate license and family privileges. See the Site Filtering section of the documentation for more information.
Field |
Data Type |
Description |
Behavior and Usage |
---|---|---|---|
Heartbeat |
Number |
The interval, in seconds, at which messages are sent to the GE Fleet message broker to ensure that the connection is kept open. |
The value in this field is 60 seconds by default. This value should not be changed unless advised by GE Digital. |
Login |
Character |
The user name that can be used to log in. |
The user for the default login account for the GE message broker server is agent2. You should use this account unless advised differently by GE. |
Port |
Number |
The port number of the GE Fleet message broker server. |
This value is set automatically when using the GE Connection workspace to configure the connection. If you are using Record Manager, the default value in this field is 5672, which is a non-SSL connection. For a SSL connection, you will need to change the value to 5671. |
Security Token |
Character | The security token. |
The security token is populated by uploading a security token file into GE Digital APM. A default security token file is created during the GE Fleet installation. |
Server |
Character |
The name of the GE Fleet message broker server. |
The default value in this field is localhost. |
SSL Certificate |
Character |
The SSL Certificate name. |
The SSL certificate is not supplied by GE Digital. It should be obtained from a third-party certificate authority. |
SSL Passphrase |
Character |
The SSL passphrase. |
This is a default setting provided by a third-party certificate authority. |
SSL Server |
Character |
The SSL Server name. |
This is a default setting provided by a third-party certificate authority. |
Use SSL |
Boolean | Indicated whether or not and SSL certificate will be used. |
If the check box is selected, the following SSL fields will be enabled, and should be configured:
|
Copyright © 2018 General Electric Company. All rights reserved.