The following diagram shows how the families used in FMEA are related to one another.
Note: In the diagram, boxes represent entity families and arrows represent relationship families that are configured in the baseline database. You can determine the direction of the each relationship definition from the direction of the arrow head: the box from which the arrow originates is the predecessor, and the box to which the arrow head points is the successor.
In the preceding diagram:
In addition to the families included in the preceding image, the following families are used by the Decision Logic Builder in FMEA:
Within the baseline GE Digital APM family hierarchy, these families are subfamilies of the GE Digital APMReference Tables family. Baseline records are provided in each of these families to support the Decision Logic Builder functionality.
The following table provides a summary of the entity families and relationship families that are used to develop an FMEA Analysis.
Records in this entity family: |
...Can be linked to records in this entity family: |
...Through a relationship definition on this relationship family: |
---|---|---|
RCM FMEA Analysis |
RCM FMEA Asset |
Has RCM FMEA Asset |
RCM FMEA Asset |
RCM FMEA Failure Mode |
Has RCM FMEA Failure Mode |
RCM FMEA Failure Effect |
RCM FMEA Recommendation |
Has RCM FMEA Recommendation |
RCM FMEA Failure Mode |
RCM FMEA Failure Effect |
Has RCM FMEA Failure Effect |
The following families and relationships are also used by FMEA but not within the analysis itself.
Records in this entity family: |
...Can be linked to records in this entity family: |
...Through this relationship: |
Purpose |
---|---|---|---|
RCM FMEA Analysis |
Human Resource |
Has RCM FMEA Team Member |
Facilitates the construction of the RCM Analysis Team Members list. Through this relationship, Human Resource records are linked directly to the RCM FMEA Analysis record. |
RCM FMEA Analysis |
RCM FMEA Task |
Has Tasks |
Allows Task records generated from Recommendation records to be linked to the RCM FMEA Analysis record for which the recommendation was created. Note that in the current version of GE Digital APM, RCM FMEA Task records cannot be created from RCM FMEA Recommendation records. Instead, RCM FMEA Recommendation records can be used to create Action records in ASM. This relationship still exists, however, to support legacy RCM FMEA Task records. |
RCM FMEA Analysis |
RCM FMEA Template |
Has Templates |
Facilitates the creation of FMEA Templates. |
RCM FMEA Asset |
Asset Strategy |
Has Strategy |
Facilitates the promotion of RCM FMEA Asset records to Asset Strategy records via Recommendation Management. This link is established when an RCM FMEA Analysis is linked to a physical or "virtual" piece of equipment or location for which you have defined Recommendation records. |
RCM FMEA Asset |
Asset Strategy Template |
Has Strategy |
Facilitates the promotion of RCM FMEA Asset records to Asset Strategy Template records via Recommendation Management. This link is established when an RCM FMEA Analysis is linked to a "virtual" piece of equipment or location for which you have defined Recommendation records. |
RCM FMEA Asset |
RCM FMEA Task |
Has Tasks |
Allows RCM FMEA Asset records to be linked to RCM FMEA Task records. This link is established only when a Task record is generated from a recommendation where the related RCM FMEA Asset record (i.e., the RCM FMEA Asset record that is linked to the RCM FMEA Analysis record) is not linked to an Equipment or Functional Location record. Note that in the current version GE Digital APM, RCM FMEA Task records cannot be created from RCM FMEA Recommendation records. Instead, RCM FMEA Recommendation records can be used to create Action records in ASM. This relationship still exists, however, to support legacy RCM FMEA Task records. |
RCM FMEA Asset |
RCM FMEA Template |
Has Templates |
Facilitates the creation of FMEA Templates. |
RCM FMEA Asset |
Task History |
Has Task History |
Facilitates the rejection of RCM FMEA Task records that are linked to RCM FMEA Asset records. When you reject an RCM FMEA Task record, a Task History record is created and linked to the RCM FMEA Asset record through the Has Task History relationship. |
RCM FMEA Failure Effect |
RCM FMEA Template |
Has Templates |
Facilitates the creation of FMEA Templates. |
RCM FMEA Failure Mode |
RCM FMEA Template |
Has Templates |
Facilitates the creation of FMEA Templates. |
RCM FMEA Recommendation |
Mitigates Risk |
Risk Assessment |
Allows you to determine how a recommendation mitigates a risk. |
RCM FMEA Recommendation |
RCM FMEA Task |
Has Tasks |
Allows RCM FMEA Recommendation records to be linked to RCM FMEA Task records that are generated from those recommendations. Note that in the current version of GE Digital APM, RCM FMEA Task records cannot be created from RCM FMEA Recommendation records. Instead, RCM FMEA Recommendation records can be used to create Action records in ASM. This relationship still exists, however, to support legacy RCM FMEA Task records. |
RCM FMEA Recommendation |
RCM FMEA Template |
Has Templates |
Facilitates the creation of FMEA Templates. |
Copyright © 2018 General Electric Company. All rights reserved.