In order to import data using the GIS Data Loader, GE Digital provides an Excel workbook, Geographic Information System (GIS).xlsx, which supports baseline GIS in GE Digital APM. This workbook must be used to perform the data load.
The following table lists the worksheets that are included in the GIS Data Loader workbook.
Worksheet | Description |
---|---|
GIS | The only worksheet used by the GIS Data Loader. It is used to load geospatial data for existing entities. |
The following table lists the fields in the workbook:
Field Caption | Field ID | Data Type (Length) | Comments |
---|---|---|---|
Batch ID | BATCH_ID | Character (50) | This is the Batch ID field. |
Entity Key | ENTITY_KEY | Numeric | This is the Entity Key field. |
Entity ID | ENTITY_ID | Character (255) | This is the Entity ID field. |
Family ID | FAMILY_ID | Character (50) | This is the Family ID field. |
Family ID Field | ID_FIELD | Character (50) | This is the ID Field name for the specified Family. |
ID | ID | Character (255) | The is the ID field. |
Geometry | GEOD_DATA | Character (4000) | This is the Spatial Data Field. |
Copyright © 2018 General Electric Company. All rights reserved.