About Reliability Centered Maintenance (RCM) Data Loader Workbook Layout and Use

This section provides a high-level overview and explanation of how the data loader workbook is constructed.

In order to import data using the Reliability Centered Maintenance (RCM) Data Loader, GE Digital provides an Excel workbook, Reliability Centered Maintenance (RCM).xlsx, which supports baseline data loading RCM analysis in GE Digital APM.

The following table lists the worksheets that are included in the Reliability Centered Maintenance (RCM) Data Loader workbook.

Worksheet

Description

Analysis

The analysis is the root record in the data model and is created first. Links to other records are established after the child record is created.

Team Members

This worksheet is used to load data into the team members for the analysis. Team members are linked to the FMEA Analysis through the Has RCM FMEA Team Member relationship.

Note: If the user wants to add team members, the individuals must already have an entry in GE Digital APM.

Functions

This worksheet is used to load data into the Functions for the analysis.

Functional Failures

This worksheet is used to load data into the Function Failures for the analysis.

Failure Modes

This worksheet is used to load data into the Failure Mode family node. The FMEA failure mode is linked directly to the virtual asset.

Failure Effects

This worksheet is used to load data into the Failure Effect family node. The failure effect is linked to both the Failure Mode and the associated recommendation. See the recommendation section for its relationship.

Recommendations

This worksheet is used to load data into the Recommendations. RCM Recommendations are linked to the associated Failure Effects. A Failure Effect can have multiple recommendations but each one must be unique.

Copyright © 2018 General Electric Company. All rights reserved.