About the Taxonomy Data Loader Workbook Layout and Use

This section provides a high-level overview and explanation of how the data loader workbook is constructed.

In order to import data using the Taxonomy Data Loader , GE Digital provides an Excel workbook, Taxonomy.xlsx, which supports baseline data loading of Taxonomy in GE Digital APM. This workbook must be used to perform the data load. On the Taxonomy worksheets, you will enter the information to load a taxonomy structure that will be assigned to assets within GE Digital APM.

The baseline file is organized such that each row is capable of creating one node in the data model when all columns contain the appropriate values.

The following table lists the worksheets that are included in the Taxonomy Data Loader workbook.

Note: Worksheets in the workbook not being used may be left blank, but should not be deleted from the workbook.

Worksheet

Description

Configuration

The Configuration worksheet is needed to describe the type of data that you will be loading and how that data should be handled during the data load.

TaxonomyCategory This worksheet is used to link Taxonomy Category data and Taxonomy Class data.
TaxonomyClass This worksheet is used to link Taxonomy Class data and Taxonomy Type data.
TaxonomyMapping This worksheet is used to link Taxonomy Type data and Taxonomy Mapping data.

Copyright © 2018 General Electric Company. All rights reserved.