About the Equipment and Functional Location Data Loader Workbook Layout and Use

This section provides a high-level overview and explanation of how the data loader workbook is constructed.

In order to import data using the Equipment and Functional Location Data Loader, GE Digital provides an Excel workbook, Equipment and Functional Location.xlsx, which supports baseline data loading of equipment and functional locations in GE Digital APM. This workbook must be used to perform the data load.

The master Excel workbook contains one worksheet for each node that will be populated in the data model.

The following table lists the worksheets that are included in the Equipment and Functional Location Data Loader workbook.

Note: Worksheets in the workbook not being used may be left blank, but should not be deleted from the workbook.

Worksheet

Description

Configuration The Configuration worksheet is needed to describe the type of data that you will be loading and how that data should be handled during the data load.

Equipment

This worksheet is used to specify data for import to the Equipment family.

FunctionalLocations

This worksheet is used to specify data for import to the Functional Location family.

FuncLocsToEquipment This worksheet is used to link existing Functional Location records to existing Equipment records.
FuncLocsToSuperiorFuncLocs This worksheet is used to link existing Functional Locations to superior Functional Locations.

Copyright © 2018 General Electric Company. All rights reserved.