Calibration Result Records

Calibration Result records store information about the fields that are defined in the Calibration Event family. This topic provides an alphabetical list and description of the fields that exist for the Calibration Result family. The information in the table reflects the baseline state and behavior of these fields.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.

Field Data Type Description Behavior and Usage
AF Error Numeric A number that corresponds to the error value in percentage recorded from the As Found value. This field is disabled and calculated based on the value in the As Found field. This field is displayed as AF Error (%) in the datasheet.
AF Pass/Fail Character A value that indicates whether the calibration has passed or failed based on whether the Overall AF Error Max value is less than or equal to the error limit.

This field is disabled and populated based on the value in the As Found Value field.

If the value in the Overall AF Error Max field is greater than the value stored in the Calibration Error Limit field, the value in this field is Fail. Otherwise, it is Pass.

AL Error Numeric A number that corresponds to the error value in percentage calculated from the As Left value. This field is disabled and calculated based on the value in the As Left field. This field is displayed as AL Error (%) in the datasheet.
AL Pass/Fail Character A value that indicates whether the calibration has passed or failed based on whether the Overall AL Error Max value is less than or equal to the error limit.

This field is disabled and populated based on the value in the As Left value field.

If the value in the Overall AL Error Max field is greater than the value stored in the Calibration Error Limit field, this value is Fail. Otherwise, this value is Pass.

As Found Value Numeric A number that indicates the As Found value of the calibration record. You can enter a value manually. The field is automatically populated for automated calibration. It is displayed as AF Value in the datasheet.
As Left Value Numeric A number that indicates the As Left value of the calibration record. You can enter this value manually. The value is auto-populated for the automated calibration. This field is displayed as AL Value in the datasheet.
Balance Content Boolean Indicates that the selected record is a balance component. You can select the component that constitutes the remaining portion other than the main components in a calibration event. This field is applicable only for Multi-Component Analyzer.

Calibration Sequence Number

Numeric A number that indicates the sequence for the calibration result record based on the selected strategy. This field displays the sequence for the result. The field is displayed as Seq No. in the datasheet.
Component Name Character Indicates the name of the component.

This field provides the standard name of the calibration result. You can enter a new name for manual calibration. The field is displayed as Standard Name in the datasheet. It is applicable for Single Component Analyzer and Multi-Component Analyzer calibrations.

Component Units Character The standard unit of measurement that is used to measure the Component.

This field contains the following values:

  • Percentage (%)
  • Parts Per Million (PPM)
  • Parts Per Billion (PPB)

This field is displayed as Standard Unit(s) in the datasheet. It is applicable for Single Component Analyzer and Multi-Component Analyzer calibrations.

Eng. Unit AF Error Numeric A number that indicates the exact value of the As Found Error in the respective engineering units. This field appears only if the value in the Error Assessment field in the Calibration record is Engineering Units in analog and discrete calibrations.
Eng. Unit AL Error Numeric A number that indicates the exact value of the As Left Error in the respective engineering units. This field appears only if the value in the Error Assessment field in the Calibration record is Engineering Units in analog and discrete calibrations.
Event ID Character The ID of the calibration event. This field is populated with a system-generated value.
Input Measure AF Numeric A number that indicates the primary As Found input value of the record. This field is automatically populated. You can, however, modify the value in this field.
Input Measure AL Numeric A number that indicates the primary As Left input value of the record. This field is automatically populated. You can, however, modify the value in this field.
Input Up/Dn Character Indicates the direction of test points of the calibration.

This field appears as Up/Dn in the datasheet.

Percentage of scale TP Numeric The percentage of scale for each test point calculated based on the strategy. You can modify this value by selecting . This field appears as % Scale in the datasheet.
Pri Output AF Numeric A number that indicates the primary As Found output value measured for calibration. This field is automatically populated and disabled in case of automated calibration. You can enter a value for manual calibration.
Primary Output AL Numeric A number that indicates the primary As Left output value measured for calibration. This field is automatically populated and disabled in case of automated calibration. You can enter a value for manual calibration.
Standard Value Numeric The expected value of the component. This field provides the standard value of the component. You can enter a new value for manual calibration. This field is applicable for Single Component Analyzer and Multi-Component Analyzer calibrations.

Copyright © 2018 General Electric Company. All rights reserved.