Calibration Profile Records

Calibration Profile records store information about the fields that are defined for the Calibration Profile family. This topic provides an alphabetical list and description of the fields that exist for the Calibration Profile family and appear on the Calibration Profile datasheet. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.

Field

Data Type

Description

Behavior and Usage

Calibration Strategy

Character

The type of strategy for the calibration.

A value is required.

This field is:

  • Blank if you created the Calibration Profile in GE Digital APM V3.6.0.0.0 or later, and then upgraded to the current version. In this case, a value is not required.
  • Enabled and populated automatically if you created the Calibration Profile in GE Digital APM V4.2.0.0.0 or later, and then upgraded to the current version.
  • Disabled and populated with the value CMX if the value in the Device Type field is CMX.
  • Disabled and blank if the value in the Device Type field is Analyzer - Multi Component.
  • Disabled and populated automatically if the value in the Device Type field is Analyzer - Single Component or Functional - Manual.
  • Enabled and blank in all other scenarios.

The list of values in this field is filtered based on the mapping ID that is associated with the selected profile template. If the mapping ID, however, does not contain a mapped strategy, then a list of all the strategies for the template type associated with the mapping ID appears in this field.

Note: If you select a Profile Template that contains Switch 1 details, and then in the Calibration Strategy field, if you select a Switch 2 strategy, a validation message appears, asking you to select a different strategy or modify the profile template. If this happens:

  • In the Calibration Strategy field, select the calibration strategy.

  • -or-

  • In the Profile Template field, select the profile template.

Device Type Character The type of calibration or calibration device.

A value is required.

This field is:

  • Blank if you created the Calibration Profile in GE Digital APM V3.6.0.0.0 or later, and then upgraded to the current version. In this case, a value is not required.
  • Enabled and populated automatically if you created the Calibration Profile in GE Digital APM V4.2.0.0.0 or later, and then upgraded to the current version.
  • Enabled and blank if you create the Calibration Profile in the current version.

On the datasheet, this field appears as a list labeled Calibration Type, and contains the following values:

  • Analog - Manual
  • Analyzer - Multi Component
  • Analyzer - Single Component
  • CMX
  • Druck DPI61x
  • Druck DPI620 (Genii)
  • Fluke 74x
  • Functional Manual
  • Switch - Manual
Is Upgraded Boolean Indicates whether the Calibration Profile was created in an earlier version of GE Digital APMor in the current version.

This check box is enabled and:

  • Selected if the Calibration Profile was created in an earlier version of GE Digital APM (i.e., before upgrading to the current version).
  • Cleared if the Calibration Profile was created in the current version.

By default, this field does not appear on the datasheet.

Profile ID Character The ID of the calibration profile.

A value is required and must be unique.

Profile Template Character The ID of the profile template.

A value is required. The list of values in this field is filtered based on the value in the Device Type field.

Copyright © 2018 General Electric Company. All rights reserved.