System Code Tables Used by Calibration Management

The following table lists the System Code Tables that are used by Calibration Management.

Table ID

Table Description

Function

MI CALIBRATION CHECKLIST TYPE MI Calibration, Check List Type Populates the Response Type field in a Calibration Template Detail, Functional Test.
MI CALIBRATION ERROR ASSESSMENT MI Calibration Error Assessment Populates the Error Assessment field in a Calibration Defaults.
MI CALIBRATION FUNCTION MI Calibration, Calibration Function Populates the Input Up/Down field in a Calibration.
MI CALIBRATION IO TYPES Calibration Input/Output Types Populates the Primary Input Range Units and Primary Output Range Units fields in a Calibration Template.
MI CALIBRATION MODE MI Calibration, Calibration Mode Populates the Input Mode and Output Mode fields in a Calibration Template.
MI CALIBRATION REFERENCES MI Calibration, Calibration List of References Populates the List of References in multiple fields.
MI CALIBRATION TEMPERATURE SOURCE MI Calibration Temperature Source Populates the Input Ref Temp Source and Output Ref Temp Source fields in a Calibration Template.
MI CALIBRATION TYPE MI Calibration, Calibration Type Populates the Calibration Type field in a Calibration Template.
MI CALIBRATION YES OR NO MI Calibration, Yes or No Populates the Response field in a Calibration, Functional Test.
MI CHARACTERISTIC CURVE MI Calibration, Characteristic Curve Populates the Input Characteristic Curve and Output Characteristic Curve fields in a Calibration (Calibration Event record).
MI CHEMICAL COMPONENTS Calibration, Chemical Components Populates the Component field in a Standard Gas Component.
MI CMX TEMPLATE INPUT METHOD CMX Standard Template Input Method Populates the Input Method field in a Calibration Template, CMX record.
MI CMX TEMPLATE INPUT TYPE CMX Template Input Type Populates the Input Type field in a Calibration Template, CMX record.
MI CMX TEMPLATE OUTPUT METHOD CMX Standard Template Output Method Populates the Output Method field in a Calibration Template, CMX record.
MI CMX TEMPLATE OUTPUT TYPE CMX Template Output Type Populates the Output Type field in a Calibration Template, CMX record.
MI DAMPING TYPE MI Calibration, Damping Type Populates the Input Damping Setting and Output Damping Setting fields in a Calibration Template.
MI ERROR BASIS MI Calibration, Percent Error Basic Calculation Populates the Percent Error Basis field in a Calibration.
MI FLUKE ERROR MODES MI Calibration, Fluke Error Modes Populates the Error Configuration field in a Calibration Template.
MI GAS CYLINDER CONNECTION NUMBER MI Calibration, Gas Cylinder Connection Number Populates the Cylinder Connection Number in a Standard Gas Cylinder.
MI GAS CYLINDER SIZE MI Calibration, Gas Cylinder Size Populates the Cylinder Size field in a Standard Gas Cylinder.
MI GAS CYLINDER TYPE MI Calibration, Gas Cylinder Type Populates the Cylinder Type field in a Standard Gas Cylinder.
MI MAINTENANCE TYPE MI Calibration, Maintenance Type Populates the Maintenance Type field in a Calibration.
MI POWER SOURCE MI Calibration, Power Source Populates the Loop Power field in a Calibration Template.
MI SENSOR TYPE MI Calibration, Sensor Type Populates the Temperature Element Type field in a Calibration Template.
MI STATUS Status Codes - CORE Populates the Template State field in a Calibration Profile Template.
MI SWITCH CONTACT STATE MI Calibration, Switch Contact State Populates the Contact State fields in a Calibration Template, Discreet record.
MI TASK TYPE REFERENCE CORE, Reference values to limit task type lists when creating tasks Populates the Task Type field in a Task record. For a Calibration Task, this field is disabled and populated with CALIBRATION.
MI TEMPERATURE MEASUREMENT STANDARD MI Calibration, Temperature Measurement Standard Populates the Temperature Standard field in a Calibration Template.
MI THERMOCOUPLE TYPE MI Calibration, Thermocouple Type Populates the Temperature Element Type field in a Calibration Template.
MI YES NO MI Core, Yes-No Populates the Performs Square Root field in a Calibration Template.
MI CALIBRATION RESULT MI_CALIBRATION_RESULT

Populates the following fields in a Calibration, CMX event:

  • Calibration Passed
  • Overall AF Pass/Fail
  • Overall AL Pass/Fail
Template Code CMX Template codes Populates the Template Code field in a Calibration Template, CMX record.
UOME Unit of measure Populates the Unit of Measure list in the Measurement Location records.

Copyright © 2018 General Electric Company. All rights reserved.