A Calibration Task record stores details about a calibration task that should be performed by a given user for Calibration Management. Specifically, these records store scheduled dates for the next time the calibrations should be performed.
Calibration Tasks are linked to Calibration Profiles. After you link a Calibration Task to one or more profiles, GE Digital APM creates a copy of the task for each Profile and Equipment combination.
For example, suppose you have two Calibration Profiles, Profile 1 and Profile 2, which are associated with Equipment as shown in the following diagram:
Note that Equipment 1 is associated with Profile 1 as well as Profile 2.
Suppose you have created Task 1 to link to all the Equipment records in Profile 1 and Profile 2. GE Digital APM creates five Calibration Tasks, and links them to the Equipment as shown in the following image. Note that since Equipment 1 is associated with both the profiles, two copies of Task 1 are linked to Equipment 1.
Each copy of the Calibration Task appears in the Calibration Queue section of the Calibration Management Overview page.
After a calibration is performed and the Calibration Event that is linked to the Equipment is closed, the Calibration Task is updated such that:
Copyright © 2018 General Electric Company. All rights reserved.