The following table provides an alphabetical list and descriptions of the fields that exist for the Work Management Item Child Definition family. The information in the table reflects the baseline state and behavior of the fields.
This family is not enabled for site filtering, which means that records in this family can be accessed by any user with the appropriate license and family privileges. See the Site Filtering section of the documentation for more information.
Field Caption |
Data Type |
Description |
Behavior and Usage |
---|---|---|---|
Child Family ID |
Character |
The successor family whose records you want to link to records belonging to the family that appears in the Family ID cell in the Work Management Item Definition record to which this Work Management Item Child Definition record is linked. |
On the datasheet, you can select a family from a list containing all families that are related to the Implementation Package family through the Has Work Management Item relationship. For example, suppose you want to be able to link Preventative Maintenance Task records to Task Grouping records. If the Family ID field in the predecessor Work Management Item Definition record contains the value Task Grouping, then in the Child Family ID list, you would select Preventative Maintenance Task. |
Child Family Relationship ID |
Character |
The relationship family that relates the family that appears in the Family ID cell in the predecessor Work Management Item Definition record to the family that is stored in the Child Family ID field in this Work Management Item Child Definition record. |
On the datasheet, you can select the appropriate relationship family from the list. |
Copyright © 2018 General Electric Company. All rights reserved.