The queries listed in the following table are provided in the Catalog folder \\Public\Meridium\Modules\Asset Strategy Management\Implementation\Queries. In this table, the values listed in the Query column refer to the query names. The baseline captions are the same as the names.
IMPORTANT: With the exception of the Get SAP ID for Equipment and Get SAP ID for Functional Location queries, you should not modify these queries in any way or move them to another Catalog folder. Also, while modifying the design of the Get SAP ID for Equipment and Get SAP ID for Functional Location queries is allowed, if you are using the baseline Equipment and Functional Location families, it is not necessary.
Query |
Behavior and Usage |
---|---|
ASI - Package Count | Returns the number of packages that currently exist in the database. |
ASI Overview Filter Query | Returns the parameters used for filtering on the ASI Overview page. |
ASI Packages - No Assets | Returns all packages in the database, but without associated assets. |
ASIAllPackages | Returns all packages that currently exist in the database. |
Asset Is Equipment |
This query is used in the ASI Action Mappings to determine if the Asset tied to the Asset Strategy is a piece of Equipment or a Functional Location. Counts greater than 0 represent Equipment where counts equal to 0 represent Functional Locations. |
Get Equipment for SAP ID |
Returns the Equipment record that contains the ID corresponding to the value supplied for the SAP Equipment ID prompt and is linked to the SAP System record identified by the value supplied for the SAP System prompt. In the baseline GE Digital APM database, the query returns records in the Equipment family. This query is not meant to be run on its own. Instead, the GE Digital APM system runs this query automatically to determine which Equipment record to link to the new Asset Strategy record when you create an Asset Strategy by importing Maintenance Items, Notifications, or Operations from SAP. When the GE Digital APM system runs this query, it performs several actions automatically:
If the query returns a record using the provided values, the GE Digital APM system links that record to the new Asset Strategy record. If the query does not return a record using that value, the GE Digital APM system runs the Get Functional Location for SAP ID query. Note: Because the documentation for importing SAP
items to create Asset Strategies assumes that you began the workflow by
importing Equipment and Functional Location records using the SAP Interfaces,
this documentation assumes that you will link your Asset Strategy records to
either an Equipment or Functional Location record. You will not, therefore,
need to modify the baseline Get Equipment for SAP ID query to include a
family other than the baseline Equipment family.
|
Get Functional Location for SAP ID |
Returns the Functional Location record that contains the ID corresponding to the value supplied for the SAP Functional Location ID prompt and is linked to the SAP System record identified by the value supplied for the SAP System prompt. In the baseline GE Digital APM database, the query returns records in the Functional Location family. This query is not meant to be run on its own. Instead, the GE Digital APM system runs this query automatically to determine which Functional Location record to link to the new Asset Strategy record when you create an Asset Strategy by importing Maintenance Items, Notifications, or Operations from SAP. When the GE Digital APM system runs this query, it performs several actions automatically:
If the query returns a record using the provided values, the GE Digital APM system links that record to the new Asset Strategy record. Note: Because the documentation for importing SAP
items to create Asset Strategies assumes that you began the workflow by
importing Equipment and Functional Location records using the SAP Interfaces,
this documentation assumes that you will link your Asset Strategy records to
either an Equipment or Functional Location record. You will not, therefore,
need to modify the baseline Get Functional Location for SAP ID query to
include a family other than the baseline Functional Location family.
|
Get Package Implemented Action Count | Returns the number of implemented actions for a particular implementation package. |
Get SAP ID for Equipment |
After providing a prompt for an Entity Key, returns the record with the provided Entity Key. In the baseline GE Digital APM database, the query returns records in the Equipment family. This query is not meant to be run on its own. Instead, GE Digital APM runs this query automatically to determine whether to populate the Equipment or Functional Location field when you build Notification or Maintenance Item records from Actions. |
Get SAP ID for Functional Location |
After providing a prompt for an Entity Key, returns the record with the provided Entity Key. In the baseline GE Digital APM database, the query returns records in the Functional Location family. This query is not meant to be run on its own. Instead, it is run automatically to determine whether to populate the Equipment or Functional Location field when you build Notification or Maintenance Item records from Actions. |
Copyright © 2018 General Electric Company. All rights reserved.