The following table provides an alphabetical list and descriptions of the fields that exist for the Execution Mapping family. The information in the table reflects the baseline state and behavior of the fields.
This family is not enabled for site filtering, which means that records in this family can be accessed by any user with the appropriate license and family privileges. See the Site Filtering section of the documentation for more information.
Field Caption |
Data Type |
Description |
Behavior and Usage |
---|---|---|---|
Class Name |
Character |
The rule class that will be invoked when you implement the Implementation Package. |
You will need to enter the name of the class. |
Description |
Text |
A description of the mapping. |
You can enter any description. |
Name |
Character |
The name of the mapping. |
The value in this field is displayed in the Execution Mapping column on the Work Management Item Definitions page. |
Project Path |
Character |
The path to the Rules Library rule project that stores the rule that will be invoked when you implement the Implementation Package. |
You will need to enter the path to the rule project. |
Copyright © 2018 General Electric Company. All rights reserved.