Calibration Setup Defaults records are used to store information about the default field values in Calibration Template families. This topic provides an alphabetical list and description of the fields that exist for the Calibration Setup Defaults family and appear on the Template Setup Defaults datasheet. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.
Field |
Data Type |
Description |
Behavior and Usage |
---|---|---|---|
Analog Error Limit |
Numeric |
The maximum amount of error in percentage that is allowed in an analog calibration. |
The value in this field is used to populate the Max Error Limit field in a Calibration Template, Analog record. |
Default Pressure Units | Character | The input and output units of measure (UOMs) for pressure in analog and discrete calibrations. |
The value in this field is used to populate the Default Pressure Units field in Calibration Template, Analog and Calibration Template, Discrete records if the value in the Input Type and Output Type fields is Pressure. |
Default Temperature Standard | Character | The temperature standard used in an analog calibration. |
The value in this field is used to populate the Temperature Standard field in a Calibration Template, Analog record. |
Default Temperature Units | Character | The input and output UOMs for temperature in analog and discrete calibrations. |
The value in this field is used to populate the Default Temperature Units field in Calibration Template, Analog and Calibration Template, Discrete records if the value in the Input Type and Output Type fields is Temperature. |
Discrete Error Limit | Numeric | The maximum amount of error, in percentage, that is allowed in a discrete calibration. |
The value in this field is used to populate the Max Error Limit field in a Calibration Template, Discrete record. |
Discrete Max Deadband | Numeric | The upper range value of deadband that is allowed in a discrete calibration. |
The value in this field is used to populate the Specified Maximum Dead Band Switch 1 and Specified Maximum Dead Band Switch 2 fields in a Calibration Template, Discrete record. |
Discrete Min Deadband | Numeric |
The lower range value of deadband that is allowed in a discrete calibration. |
The value in this field is used to populate the Specified Minimum Dead Band Switch 1 and Specified Minimum Dead Band Switch 2 fields in a Calibration Template, Discrete record. |
Error Assessment | Character | The maximum amount of error in engineering units that is allowed in a discrete calibration. |
The value in this field is used to populate the Engineering Units Error Limit field in a Calibration Template, Discrete record. |
Input Damping Setting | Character | Indicates whether input damping is on or off. |
The value in this field is used to populate the Input Damping Setting field in Calibration Template, Analog and Calibration Template, Discrete records. |
Input Increment | Numeric |
The incremented source value in an automated calibration. |
The value in this field is used to populate the Input Increment field in Calibration Template, Analog and Calibration Template, Discrete records. |
Input Min Max Mode | Character | Indicates whether input min max mode is on or off. |
The value in this field is used to populate the Input Min Max Mode field in Calibration Template, Analog and Calibration Template, Discrete records. |
Input Ref Temp Source | Character |
The internal temperature reference in an automated calibration. |
The value in this field is used to populate the Input Ref Temp Source field in Calibration Template, Analog and Calibration Template, Discrete records. |
Input Simulation Delay | Numeric |
The per-step delay, in milliseconds, after the input simulation is updated to compensate for settling and lag. |
The value in this field is used to populate the Input Simulation Delay field in Calibration Template, Analog and Calibration Template, Discrete records. |
MC Analyzer Error Limit | Numeric | The maximum percentage of error that is allowed in a multi-component analyzer calibration. |
The value in this field is used to populate the Max Error Limit field in a Calibration Template, Multi-Component Analyzer record. |
Output Damping Setting | Character | Indicates whether output damping is on or off. |
The value in this field is used to populate the Output Damping Setting field in Calibration Template, Analog and Calibration Template, Discrete records. |
Output Ref Temp Source | Character | The external temperature reference in an automated calibration. |
The value in this field is used to populate the Output Ref Temp Source field in Calibration Template, Analog and Calibration Template, Discrete records. |
Ramp Time | Numeric | The ramp time, in seconds, in a discrete calibration. |
This field is disabled for Fluke devices. The value in this field is used to populate the Ramp Time field in a Calibration Template, Discrete record. |
Repeat Count | Numeric | The number of test cycles to perform a discrete calibration. |
The value in this field is used to populate the Repeat Count field in a Calibration Template, Discrete record. |
SC Analyzer Error Limit | Numeric | The maximum error limit that is allowed in a single component analyzer and a multi-component analyzer calibration. |
The value in this field is used to populate Max Error Limit field in the Calibration Template, Multi-Component Analyzer and Calibration Template, Single Component Analyzer records. |
Validate Deadband | Boolean | Indicates whether or not you want the GE Digital APM system to consider the deadband range values to determine if a discrete calibration has passed or failed. |
The value in this field is used to populate the Validate Deadband field in the Calibration Template, Discrete record. |
Weight Scale Error Limit | Numeric | The maximum amount of error, in percentage, that is allowed in a weight scale calibration. |
The value in this field is used to populate the Max Error Limit field in a Calibration Template, Weight Scale record. |
Copyright © 2018 General Electric Company. All rights reserved.