Passive IPL Records

Passive IPL records store information about the probability of failure of various types of passive IPLs. This topic provides an alphabetical list and description of the fields that exist for the Passive IPL family. The information in the table reflects the baseline state and behavior of these fields.

IMPORTANT: The records in this family can be modified only by users who belong to the Security Groups MI SIS Administrator or MI HA Administrator.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.

Field

Data Type

Description

Behavior and Usage

Default Value

Numeric

Indicates the default probability that the Passive IPL will fail to mitigate the risk.

You can enter a value manually.

Lower Range Numeric Indicates the lower range for the probability that the Passive IPL will fail to mitigate the risk.

You can enter a value manually.

Passive IPL ID Character Identifies the type of Passive IPL.

This field appears a list that is populated by the MI_PASSIVE_IPL System Code Table.

Upper Range Numeric Indicates the upper range for the probability that the Passive IPL will fail to mitigate the risk.

You can enter a value manually.

Related Information

Copyright © 2018 General Electric Company. All rights reserved.