The GE Digital APM Rule Library contains a baseline rule that defines the mapping between Action data and Inspection Task, Calibration Task or EAM data. Follow these steps if you need to modify this mapping.
Tip: EAM Action mapping is for controlling the mappings between Action data and the EAM Notifications via the Implement as EAM Work Request and EAM Maintenance Plan features. Using Action Mappings, you can send Action information to your EAM system as a singular task or a recurring maintenance plan.
Steps
Select the Action Mappings tab.
The Action Mappings workspace appears.
Select the hyperlink associated with the mapping that you want to modify.
The Project Path and Class Name for the Action Mapping associated with your selection appear.
In the Project Path box, enter the path to the rule project that contains the mapping you want to use.
Select
Your configuration is saved. The mappings defined in the specified rule project are now used to map Action data to Inspection Task, Calibration Task, or EAM data.
Copyright © 2018 General Electric Company. All rights reserved.