Modify the High Loss Value

The High Loss value is used to determine if the percentage of decrease in the measurement value from the previous measurement is greater than or equal to the High Loss value. By default, the value in the High Loss field is 30 percent. This topic describes how to modify this value.

Steps

  1. Access the Global Preferences workspace.
  2. In the upper-right corner of the workspace, select .

    The boxes and check boxes in the Global Preferences workspace are enabled. is replaced with .

  3. In the Color-Coding Preferences section, in the High Loss box, enter a value between 0 and 100.
  4. In the upper-right corner of the page, select .

    The High Loss value is modified.

Results

Related Information

Copyright © 2018 General Electric Company. All rights reserved.