Initiating Event Records

Initiating Event records are used to determine the frequency of occurrence of an initiating event. This topic provides an alphabetical list and description of the fields that exist for the Initiating Event family and appear on the LOPA datasheet. The information in the table reflects the baseline state and behavior of these fields.

This family is not enabled for site filtering, which means that records in this family can be accessed by any user with the appropriate license and family privileges. See the Site Filtering section of the documentation for more information.

Field

Data Type

Description

Behavior and Usage

Default Value Numeric Indicates the default value for the frequency of the Initiating Event.

You can enter a value manually.

This field populates the following fields:

  • Frequency of Initiating Event field on the LOPA datasheet
  • Cause Frequency (per year) field on the Hazards Analysis Cause datasheet.
Initiating Event ID Character Identifies the type of Initiating Event. This field appears a list that is populated by the INIT_EVENT System Code Table.
Lower Boundary Numeric Indicates the lower boundary value for the frequency of the Initiating Event.

You can enter a value manually.

Upper Boundary Numeric Indicates the upper boundary value for the frequency of the Initiating Event.

You can enter a value manually.

Related Information

Copyright © 2018 General Electric Company. All rights reserved.