GAA Plant Records

GAA Plant records store information about the fields that are defined for the GAA Plant family in the baseline GE Digital APM database. This topic provides an alphabetical list and description of the fields that exist for the GAA Plant family and appear on the Plant section. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.

Field Data Type Description Behavior and Usage
Address 1 Character Identifies the first line of the address of the plant.

You can enter a value manually. We recommend that you use the address that is on file with the Regulatory Organization.

This field is available in the Plant section.

Address 2 Character Identifies the second line of the address of the plant.

You can enter a value manually. We recommend that you use the address that is on file with the Regulatory Organization.

This field is available in the Plant section.

Area Character Used to group GAA Plants into an area.

A baseline rule exists to populate this field with a list of each unique value that exists in the Area field in all other GAA Plants.

You can enter a value manually.

When you enter a value in the Area field for one GAA Plant, the value will be available in the Area drop-down for next plant.

This field is available in the Plant section.

Asset ID Character Identifies the Functional Location associated with the GAA Plant.

You can select a Functional Location to associate with the GAA Plant.

This field is required.

City Character Identifies the city in which the plant resides.

You can enter a value manually. We recommend that you use the city associated with the address that is on file with the Regulatory Organization.

This field is available in the Plant section.

Company ID Character Identifies the company that owns the plant.

When a GAA Plant is created, this field is populated automatically with the value in the Company ID field in the GAA Company to which the GAA Plant is linked.

This field is available in the Plant section.

Company Name Character Identifies the full name of the company that owns the plant.

When a GAA Plant is created, this field is populated automatically with the value in the Company Name field in the GAA Company to which the GAA Plant is linked.

This field is available in the Plant section.

Country Character Indicates the country in which the plant resides.

You can enter a value manually. We recommend that you use the country associated with the address that is on file with the Regulatory Organization.

This field is available in the Plant section.

Organization Character Identifies the organization to which the plant belongs.

You can enter a value manually. After you enter a value in the Organization field for one GAA Plant, the Organization value will be available in the drop-down list for the next plant. Therefore, when you create a new plant, you can either enter a new value or select the Organization value for an existing plant in the list.

This field is available in the Plant section.

Plant ID Character Identifies the plant and is used to populate the Record ID.

This field is required for all GAA Plants.

This field is available in the Plant section.

Plant Name Character Identifies the full name of the plant and is used to populate the Record ID.

This is a character field that is required for all GAA Plants. This value is defined by the Regulatory Organization.

This field is available in the Plant section.

Primary Plant Code Character Identifies the code that is assigned to the GAA Plant by the regulatory body selected in the Primary Regulatory Body field of the GAA Company record.

You can enter a value manually.

This field is required.

Primary Regulatory Body Character Identifies the first council to which data will be reported.

A baseline rule exists to populate this field based on your selection in the Primary Regulatory Body field in the GAA Company recorda dn is disabled.

This field is available in the Plant section.

Secondary Plant Code Character Identifies the code that is assigned to the GAA Plant by the regulatory body selected in the Secondary Regulatory Body field of the GAA Company record.

This field is required only if the Primary Regulatory Organization is CEA and is disabled.

Secondary Regulatory Body Character Identifies the second council to which data will be reported.

The Plant family inherits Secondary Regulatory Body field from the Company.

This field is available in the Plant section.

State Character Indicates the state in which the plant resides.

A baseline rule exists to populate this field with a list of System Codes in the MI_GM_STATE System Code Table. We recommend that you use the state associated with the address that is on file with the Regulatory Organization.

This field is available in the Plant section.

Time Zone Character Indicates the time zone to which the GAA Plant is associated.

By default, this field is set to Eastern Standard Time. You can select a time zone from the available list of time zones.

This field is available in the Plant section.

This field is required.

Use Daylight Saving Time Boolean

Indicates whether Daylight Saving Time should be used in records that are associated with the GAA Plant.

If the value in this field is:

  • True, Daylight Saving Time will be adjusted automatically.
  • False, Daylight Saving Time will not be adjusted automatically.

This field is available in the Plant section.

Zip Code Character Identifies the zip code of the location of the plant.

You can enter a value manually. We recommend that you use the zip code associated with the address that is on file with the Regulatory Organization.

This field is available in the Plant section.

Copyright © 2018 General Electric Company. All rights reserved.