GAA Event Transition Records

GAA Event Transition records store information about the fields that are defined for the GAA Event Transition family in the baseline GE Digital APM database. This topic provides an alphabetical list and description of the fields that exist for the GAA Event Transition family. The information in the table reflects the baseline state and behavior of these fields.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.

Field Data Type Description Behavior and Usage
From Event Type Character The type of the parent event between the two events in transition. A value is required. This field appears as a list that is populated by values in the Event Type Code field in each GAA Event Type record.
To Event Type Character The type of the related event between the two events in transition.

A value is required. This field appears as a list that is populated by values in the Event Type Code field in each GAA Event Type record.

The value in this field is used to populate the Capacity Event Type field in the related event based on the value in the Capacity Event Type, Cause Code, and Net Derate Amount fields in the parent event.

Validation Rule Character The rule that should be applied for the two events to be in transition. As per Canadian Electricity Association (CEA) guidelines, events of certain event types can be in transition only if certain conditions are satisfied. GE Digital APM validates if the condition that you enter in this field is satisfied. If not, a message appears below the Capacity Event Type box on the Related Event datasheet specifying the condition that must be satisfied.

Copyright © 2018 General Electric Company. All rights reserved.