GAA Code Mapping Records

GAA Code Mapping records store information about fields that are defined for the GAA Code Mapping family in the baseline GE Digital APM database. This topic provides an alphabetical list and description of the fields that exist for the GAA Code Mapping family and appear on the datasheet. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.

This family is not enabled for site filtering, which means that records in this family can be accessed by any user with the appropriate license and family privileges. See the Site Filtering section of the documentation for more information.

Field

Data Type

Description

Behavior and Usage

CEA Amplification Code Character

Indicates the CEA Amplification Code for the selected Unit type.

This field is populated using the following format:

<AmplificationCode>(<Description>)

Where,

  • <Description> is the value in the Description field in the Amplification Code record, which has Regulatory Organization field set to Canadian Electricity Association (CEA).
  • <AmplificationCode> is the value in the Amplification Code field in the Amplification Code record, which has Regulatory Organization field set to Canadian Electricity Association (CEA).

You can select a value from the available CEA Amplification Codes for the selected Unit Type.

The available values appear in this field only after you select a value in the CEA Unit Type field.

CEA Cause Code Character

Indicates the CEA Outage Code for the selected Unit type.

This field is populated using the following format:

<Code> ~ <Code Description>

Where,

  • <Code> is the value in the Code field in the Cause Code record.
  • <Code description> is the value in the Code Description field in the Cause Code record.

You can select value (s) from the available CEA Outage Codes for the selected Unit Type.

The available values appear in this field only after you select a value in the CEA Unit Type field.

This field is required.

CEA Unit Type Character

Indicates the type of Unit available for CEA.

You can select a type of Unit from the list of available options.

This field is required.

NERC Amplification Code Character Indicates the NERC Amplification Code for the selected Unit type.

This field is populated using the following format:

<AmplificationCode>(<Description>)

Where,

  • <Description> is the value in the Description field in the Amplification Code record, which has Regulatory Organization field set to North American Electric Reliability Corporation (NERC).
  • <AmplificationCode> is the value in the Amplification Code field in the Amplification Code record, which has Regulatory Organization field set to North American Electric Reliability Corporation (NERC).

You can select a value from the available NERC Amplification Codes for the selected Unit Type.

NERC Cause Code Character

Indicates the NERC Cause Code for the selected Unit type.

This field is populated using the following format:

<Code> ~ <Code Description>

Where,

  • <Code> is the value in the Code field in the Cause Code record, which has Regulatory Organization field set to North American Electric Reliability Corporation (NERC).
  • <Code description> is the value in the Code Description field in the Cause Code record, which has Regulatory Organization field set to North American Electric Reliability Corporation (NERC).

You can a select value from the available NERC Cause Code for the selected Unit Type.

This field is required.

Copyright © 2018 General Electric Company. All rights reserved.