Define Readings Preferences

Steps

  1. Access the Global Preferences workspace.
  2. In the upper-right corner of the workspace, select .

    The boxes and check boxes in the Global Preferences workspace are enabled. is replaced with .

  3. In the Readings Preferences section, in the Reading Tolerance box, enter the value that defines the range within which readings must fall in order to pass evaluation.

  4. In the Readings Calculation Method box, select the value that indicates how you want Thickness Measurement values to be calculated based upon the values in the Readings field. You can choose Average, Minimum, Maximum, or Custom.
  5. If you select Custom, to the right of the Custom Rule for Readings Calculation box, select .

    The Select a Project and Method from the Catalog window appears.

  6. In the left pane of the window, navigate to and select the Rules Library folder containing the project in which the desired rule is defined.

    The middle pane is populated with a list of projects that exist in the selected folder.

  7. In the middle pane, select the project that contains the method that you want to use for the readings calculation rule.

    The right pane is populated with a list of valid methods.

  8. In the right pane, select the method.
  9. Select Done.

    The Select a Project and Method from the Catalog window closes.

  10. In the upper-right corner of the workspace, select .

    The custom readings calculation settings are saved along with any other changes to the settings on the Global Preferences workspace.

Copyright © 2018 General Electric Company. All rights reserved.