Steps
Select
In the Global Preferences workspace, the boxes and check boxes are enabled.
In the Custom Corrosion Rate Options section, below the Custom Corrosion Rate A heading, in the Label box, enter the label that you want to use for this custom corrosion rate.
To the right of the Calculation Rule box, select
The Select a Project and Method from the Catalog window appears.
Tip: If you know the path to the method, you can also enter it directly in the Calculation Rule box.
In the left pane of the window, navigate to and select the Rules Library folder containing the project in which the desired rule is defined.
The middle pane is populated with a list of projects that exist in the selected folder.
In the middle pane, select the project that contains the method that you want to use for the corrosion rate rule.
The right pane is populated with a list of valid methods.
Select Done.
The Select a Project and Method from the Catalog window closes.
In the upper-right corner of the workspace, select
The custom corrosion rate settings are saved along with any other changes to the settings on the Global Preferences workspace.
Copyright © 2018 General Electric Company. All rights reserved.