Consequence Adjustment Probability records are used to determine the probability that a conditional modifier event may occur, thereby adjusting the frequency of unmitigated consequence. This topic provides an alphabetical list and description of the fields that exist for the Consequence Adjustment Probability family and appear on the Conditional Modifier datasheet. The information in the table reflects the baseline state and behavior of these fields. These records in this family can be modified only by users who belong to the Security Groups MI SIS Administrator or MI HA Administrator.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Field |
Data Type |
Description |
Behavior and Usage |
---|---|---|---|
Default Value | Numeric | Indicates the default value for probability of occurrence of the conditional modifier. | You can enter a value manually. |
Modifier ID | Character | Identifies the type of conditional modifier. |
This field appears a list that is populated by the MI_CONSQ_ADJ_PROB System Code Table. |
Copyright © 2018 General Electric Company. All rights reserved.