Calibration Template, Weight Scale Records

Calibration Template, Weight Scale records store details on the weight scale calibration that should be performed for a specific piece of equipment. This topic provides an alphabetical list and description of the fields that exist for the Calibration Template, Weight Scale family and appear on the Calibration Weight Scale Template Setup datasheet. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.

Field Name Data Type Description Behavior and Usage
Asset Key Numeric The Entity Key of the Equipment to which the Calibration Template is linked. This field is used by the GE Digital APM system and should not be modified. This field does not appear on a datasheet by default. When you apply a Calibration Template to an Asset, the details of the Asset are retrieved based on the value in the Asset Key field.
Calibration Task ID Character The ID of the Calibration Task that is linked to the Equipment to which the Calibration Template is linked. This field contains the IDs of the Calibration Task that are linked to the Equipment to which the Calibration Template is linked. You can select the required Calibration Task from the list. If the Equipment is not linked to a Calibration Task, this list will be empty.
Calibration Type Character The type of calibration for which you are creating the template.

This field is disabled and populated with the value ANALOG-MANUAL by default.

Input Type Character The input type for the weight scale calibration.

This field appears as a list that is populated by the MI CALIBRATION IO TYPES System Code Table. You can choose from the following input types:

  • Weight
  • Voltage

  • Current

  • Other

This field is required.

Manufacturer Character The manufacturer of the Equipment that is linked to the Calibration Template. This field is disabled and populated with the value stored in the Manufacturer field in the Equipment that is linked to the Calibration Template. If you have accessed the template from the library, then this field is disabled and blank.
Max Error Limit Numeric A number that represents the maximum amount of error in percent that is allowed before a calibration event is considered failed.

This field is populated with a default value, as specified in the Weight Scale Error Limit field in the Calibration Setup Defaults record.

This field includes an additional label PCT to the right. This field is populated with the value specified in the Weight Scale Error Limit field in the Calibration Setup Defaults record. You can modify this value if required.

Model Number Character The model number of the Equipment that is linked to the Calibration Template. This field is disabled and populated with the value stored in the Model Number field in the Equipment that is linked to the Calibration Template. If you have accessed the template from the library, then this field is disabled and blank.
Output Type Character The output type for the weight scale calibration.

This field appears as a list that is populated by the MI_CALIBRATION_IO_TYPES System Code Table. You can choose from the following output types:

  • Pressure

  • Temperature

  • Flow

  • Level

  • Weight

  • Voltage

  • Current

  • Frequency

  • Resistance

  • Other

This field is required.

Primary Input LRV Numeric A number representing the lower range value for the primary input range.

This field is grouped with the following other fields in the Primary Input Details section:

  • Primary Input URV
  • Primary Input Range Units

The value stored in the Primary Input LRV field combined with the value stored in the Primary Input URV field define the primary input range for the calibration. This field is required.

Primary Input Range Units Character The units of measure (UOM) for the primary input.

This field is grouped with the following other fields in the Primary Input Details section:

  • Primary Input LRV
  • Primary Input URV

This field contains a list of units of measure that is filtered based on the value in the Input Type field. This means that only the UOM values that are relevant for that input type will appear in the list. After you select a value in this list, the GE Digital APM system checks to see if the UOM is compatible with the Fluke device. If the selected value is not compatible, an error message will appear, indicating the problem.

Primary Input URV Numeric A number representing the upper range value for the primary input range.

This field is grouped with the following other fields in the Primary Input Details section:

  • Primary Input LRV

  • Primary Input Range Units

The value stored in the Primary Input URV field combined with the value stored in the Primary Input LRV field define the primary input range for the calibration. This field is required.

Primary Output LRV Numeric A number representing the lower range value for the primary output range.

This field is grouped with the following other fields in the Primary Output Details section:

  • Primary Output URV

  • Primary Output Range Units

The value stored in the Primary Output LRV field combined with the value stored in the Primary Output URV field define the primary output range for the calibration. This field is required.

Primary Output Range Units Character The units of measure for the primary input.

This field is grouped with the following other fields in the Primary Output Details section:

  • Primary Output LRV

  • Primary Output URV

This field contains a list of units of measure that is filtered based on the value in the Output Type field. This means that only the UOM values that are relevant for that output type will appear in the list. After you select a value in this list, the GE Digital APM system verifies if the UOM is compatible with the Fluke device. If the selected values is not compatible, an error message will appear, indicating the problem. This field appears as a list that is populated by the MI_CALIBRATION_IO_TYPES System Code Table.

Primary Output URV Numeric A number representing the upper range value for the primary output range.

This field is grouped with the following other fields in the Primary Output Details section:

  • Primary Output LRV

  • Primary Output Range Units

The value stored in the Primary Output URV field combined with the value stored in the Primary Output LRV field define the primary ouput range for the calibration. This field is required.

Refresh Equipment Data Boolean Indicates whether or not information in the Equipment that is linked to the Calibration Template has been updated. This field is used by the GE Digital APM system and should not be modified. This field does not appear on a datasheet by default.
Serial Number Character The serial number of the Equipment that is linked to the Calibration Template.

This field is disabled and populated with the value stored in the Serial Number field in the Equipment that is linked to the Calibration Template. If you have accessed the template from the library, then this field is disabled and blank.

Tag Description Character The description of the piece of equipment, which is represented by the Equipment that is linked to the Calibration Template. This field is disabled and populated with the value stored in the Equipment Short Description field in the Equipment that is linked to the Calibration Template. If you have accessed the template from the library, then this field is disabled and blank.
Tag Name Character The ID of the Equipment that is linked to the Calibration Template. This is the Equipment Technical Number of the asset. This field is disabled and populated with the value in the Equipment field in the Equipment record that is linked to the Calibration Template. If you have accessed the template from the library, then this field is disabled and blank.
Template State Character The state of the Calibration Template.

This field contains the following values:

  • Development
  • Approved

  • Obsolete

By default, this field contains the value Development.

Related Information

Copyright © 2018 General Electric Company. All rights reserved.