Calibration Template, Analyzer Multi-Component records store details on the multi-component analyzer calibration that should be performed for a specific piece of equipment. This topic provides an alphabetical list and description of the fields that exist for the Calibration Template, Multi-Component Analyzer family. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Field Name | Data Type | Description | Behavior and Usage |
---|---|---|---|
Asset Key | Numeric | The Entity Key of the Equipment that is linked to the Calibration Template. This field is used by the GE Digital APM system and should not be modified. | This field does not appear on a datasheet by default. When you apply a Calibration Template to an Asset, the details of the Asset are retrieved based on the value in the Asset Key field. |
Calibration Task ID | Character | The ID of the Calibration Task that is linked to the Equipment to which the Calibration Template is linked. | This list contains the IDs of the Calibration Tasks that are linked to the Equipment to which the Calibration Template is linked. If the Equipment is not linked to a Calibration Task, this list will be empty. |
Calibration Type | Character | The type of calibration for which you are creating the template. |
This field is disabled and populated with the value ANALYZER-MULTI COMPONENT by default. |
Manufacturer | Character | The manufacturer of the Equipment that is linked to the Calibration Template. | This field is disabled and populated with the value stored in the Manufacturer field in the Equipment that is linked to the Calibration Template. If you have accessed the template from the library, then this field is disabled and blank. |
Max Error Limit | Numeric | A number representing the maximum percentage of error that is allowed before a calibration event is considered failed. |
This field is populated with the value specified in the SC Analyzer Error Limit field in the Calibration Setup Defaults record. You can modify this value if required. |
Model Number | Character | The model number of the Equipment that is linked to the Calibration Template. | This field is disabled and populated with the value stored in the Model Number field in the Equipment that is linked to the Calibration Template. If you have accessed the template from the library, then this field is disabled and blank. |
Refresh Equipment Data | Boolean | Indicates whether or not information in the Equipment that is linked to the Calibration Template has been updated. This field is used by the GE Digital APM system and should not be modified. | This field does not appear on a datasheet by default. |
Serial Number | Character | The serial number of the Equipment that is linked to the Calibration Template. |
This field is disabled and populated with the value stored in the Serial Number field in the Equipment that is linked to the Calibration Template. If you have accessed the template from the library, then this field is disabled and blank. |
Tag Description | Character | The description of the Equipment to which the Calibration Template is linked. | This field is disabled and populated with the value stored in the Equipment Short Description field in the Equipment that is linked to the Calibration Template. If you have accessed the template from the library, then this field is disabled and blank. |
Tag Name | Character | The ID of the Equipment to which the Calibration Template is linked. | This field is disabled and populated with the value in the Equipment field in the Equipment record that is linked to the Calibration Template. If you have accessed the template from the library, then this field is disabled and blank. |
Template ID | Character | The ID for the record. | This field is required and must be unique. |
Template State | Character | The state of the Calibration Template. |
This list contains the following values:
The default value is Development. |
Copyright © 2018 General Electric Company. All rights reserved.