Calibration Template, CMX Records

Calibration Template, CMX records store details about the calibration that must be performed for a specific piece of equipment using CMX software. This topic provides an alphabetical list and description of the fields that exist for the Calibration Template, CMX family. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.

This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.

Field

Data Type

Description

Behavior and Usage

Asset Key Numeric The Entity Key of the piece of equipment to which the Calibration Template is linked.

This field does not appear on a datasheet by default. When you apply a Calibration Template to an Asset, the details of the Asset are retrieved based on the value in the Asset Key field.

This field is used by the GE Digital APM system, and should not be modified.

Calibration Type Character The type of calibration you will perform.

This field is disabled, and contains the value CMX by default.

This field is required.

Input Method Character The method for sending input measures to the piece of equipment that is being calibrated.

This field appears as a list that is populated by the MI_CMX_TEMPLATE_INPUT_METHOD System Code Table.This field contains a list of the following input methods:

  • Controlled (Controlled)
  • Controlled and Measured (Controlled and Measured)
  • Keyed (Keyed)
  • Measured (Measured)
  • Sourced (Sourced)
  • N/A (N/A)

This field is required.

Input Type Character The type of input for the calibration to be performed.

This field appears as a list that is populated by the MI_CMX_TEMPLATE_INPUT_TYPE System Code Table. This field contains a list of the following input types:

  • CHECKLIST (CHECKLIST)
  • ELECTRICAL (ELECTRICAL)
  • MASS (MASS)
  • PRESSURE (PRESSURE)
  • TEMPERATURE (TEMPERATURE)
  • VALUE (VALUE)
  • N/A (N/A)

This field is required.

Max Error Limit Numeric A number representing the maximum amount of error in percent that is allowed before a calibration event is considered failed.

This field is populated with the value 3 by default. You can modify this value if needed.

This value is used in the calibration to calculate whether a calibration event has failed or passed.

Output Method Character The method for capturing output measures from the piece of equipment that is being calibrated.

This field appears as a list that is populated by the MI_CMX_TEMPLATE_OUTPUT_METHOD System Code Table.This field contains a list of the following output method:

  • Keyed (Keyed)
  • Measured (Measured)
  • FOUNDATION H1 (FOUNDATION H1)
  • HART (HART)
  • PROFIBUS PA (PROFIBUS PA)
  • N/A (N/A)

This field is required.

Output Type Character The type of output for the calibration.

This field appears as a list that is populated by the MI_CMX_TEMPLATE_OUTPUT_TYPE System Code Table.This field contains a list of the following output types :

  • ELECTRICAL (ELECTRICAL)
  • MASS (MASS)
  • PRESSURE (PRESSURE)
  • STATE (STATE)
  • TEMPERATURE (TEMPERATURE)
  • VALUE (VALUE)
  • N/A (N/A)

This field is required.

Primary Input LRV Numeric A number representing the lower range value for the primary input range.

This field appears in the Primary Input Details subsection of the Equipment Details section.

The value stored in the Primary Input LRV field combined with the value stored in the Primary Input URV field defines the primary input range for the calibration.

This field is disabled if you selected one of the following values in the Template Code field:

  • Checklist (cl) 
  • Checklist, IEC60079-17, Table 1 (c6007917_1)
  • Checklist, IEC60079-17, Table 2 (c6007917_2)

For other values of Template Code, this field is required.

Primary Input Range Units Character The units of measure for the primary input.

This field contains a list of Units of Measurements.

This field is disabled if you selected one of the following values in the Template Code field:

  • Checklist (cl) 
  • Checklist, IEC60079-17, Table 1 (c6007917_1)
  • Checklist, IEC60079-17, Table 2 (c6007917_2)

For other values of Template Code, this field is required.

Primary Input URV Numeric A number representing the upper range value for the primary input range.

This field appears in the Primary Input Details subsection of the Equipment Details section.

The value stored in the Primary Input URV field combined with the value stored in the Primary Input LRV field defines the primary input range for the calibration.

This field is disabled if you selected one of the following values in the Template Code field:

  • Checklist (cl) 
  • Checklist, IEC60079-17, Table 1 (c6007917_1)
  • Checklist, IEC60079-17, Table 2 (c6007917_2)

For other values of Template Code, this field is required.

Primary Output LRV Numeric A number representing the lower range value for the primary output range.

This field appears in the Primary Output Details subsection of the Equipment Details section.

The value stored in the Primary Output LRV field combined with the value stored in the Primary Output URV field defines the primary output range for the calibration.

This field is disabled if you selected one of the following values in the Template Code field:

  • Checklist (cl) 
  • Checklist, IEC60079-17, Table 1 (c6007917_1)
  • Checklist, IEC60079-17, Table 2 (c6007917_2)
  • Electrical Switch (es)
  • Pressure Switch (ps)
  • Temperature Switch (ts)

For other values of Template Code, this field is required.

Primary Output Units Character The units of measure for the primary input.

This field contains a list of Units of Measurements.

This field is disabled if you selected one of the following values in the Template Code field:

  • Checklist (cl) 
  • Checklist, IEC60079-17, Table 1 (c6007917_1)
  • Checklist, IEC60079-17, Table 2 (c6007917_2)
  • Electrical Switch (es)
  • Pressure Switch (ps)
  • Temperature Switch (ts)

For other values of Template Code, this field is required.

Primary Output URV Numeric A number representing the upper range value for the primary output range.

This field appears in the Primary Output Details subsection of the Equipment Details section.

The value stored in the Primary Output URV field combined with the value stored in the Primary Output LRV field defines the primary output range for the calibration.

This field is disabled if you selected one of the following values in the Template Code field:

  • Checklist (cl) 
  • Checklist, IEC60079-17, Table 1 (c6007917_1)
  • Checklist, IEC60079-17, Table 2 (c6007917_2)
  • Electrical Switch (es)
  • Pressure Switch (ps)
  • Temperature Switch (ts)

For other values of Template Code, this field is required.

Switch Set Point Character Indicates the value (i.e., pressure, temperature, or electrical output) at which the switch changes state.

This field appears in the Primary Output Details subsection of the Equipment Details section.

If you selected one of the following values in the Template Code field, then this field is enabled and required:

  • Pressure Switch (ps)
  • Temperature Switch (ts)

  • Electrical Switch (es)

For other values of Template Code, this field is disabled.

Switch Reset Point Numeric Indicates the value (i.e., pressure, temperature, or electrical output) at which the switch resets to normal state.

This field appears in the Primary Output Details subsection of the Equipment Details section.

If you selected one of the following values in the Template Code field, then this field is enabled and required:

  • Pressure Switch (ps)
  • Temperature Switch (ts)

  • Electrical Switch (es)

For other values of Template Code, this field is disabled.

Switch Set Action Numeric Indicates the state that the switch must change to, when the value (i.e., pressure, temperature, or electrical output) is at the set point.

This field appears in the Primary Output Details subsection of the Equipment Details section.

This field contains a list of the following values:

  • Opens
  • Closes

If you selected one of the following values in the Template Code field, then this field is enabled and required:

  • Pressure Switch (ps)
  • Temperature Switch (ts)

  • Electrical Switch (es)

For other values of Template Code, this field is disabled.

Template Code Character Identifies the corresponding template type in CMX Software.

This field appears as a list that is populated by the Template_Code System Code Table.

The template codes contain a value that can map the template to the corresponding template type in the CMX software.

Based on your selection in this field, the fields in the Equipment Details section of the datasheet are either enabled or disabled.

This field is required.

Template ID Character The Identification of the Calibration Template. This field is required and must be unique.
Template State Character The state of the Calibration Template.

This field contains the value Development by default. You can select one of following values in this field:

  • Development (Development)
  • Approved (Approved)
  • Obsolete (Obsolete)

Related Information

Copyright © 2018 General Electric Company. All rights reserved.