Calibration Template, Analog records store details on the analog calibration that should be performed for a specific piece of equipment. This topic provides an alphabetical list and description of the fields that exist for the Calibration Template, Analog family. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Field | Data Type | Description | Behavior and Usage |
---|---|---|---|
Asset Key | Numeric | The Entity Key of the Equipment to which the Calibration Template is linked. This field is used by the GE Digital APM system, and should not be modified. | This field does not appear on a datasheet by default. When you apply a Calibration Template to an Asset, the details of the Asset are retrieved based on the value in the Asset Key field. |
Calibration Type | Character | The type of calibration for which you are creating the template. |
This field is disabled and populated based on the type of template that you selected on the Profile Template page. This field is populated with one of the following values:
|
Custom Input Lower Range | Numeric | A number representing the lower range value for the custom input range. | This field appears on the datasheet as a text box labeled Low, and is grouped with the following other fields in the Custom Input Details subsection:
|
Custom Input Range UOM | Character | The units of measure for the custom input range. | This field appears on the datasheet as a list labeled UOM, and is grouped with the following other fields in the Custom Input Details subsection:
If the Calibrator Type field contains the value Druck DPI620 (Genii) or Druck DPI61x, then this list is filtered by the value that you select in the Input Type field. This field is enabled and required only when the Custom Input Values check box is selected. This field appears as a list that is populated by the MI_CALIBRATION_IO_TYPES System Code Table. |
Custom Input Upper Range | Numeric | A number representing the upper range value for the custom input range. | This field appears on the datasheet as a text box labeled High, and is grouped with the following other fields in the Custom Input Details subsection:
|
Custom Input Values | Boolean | Indicates that you will enter custom input values for the calibration. |
This field is enabled only when the value stored in the Calibration Type field is FLUKE 74x. When you select the Custom Input Values check box:
|
Custom Output Lower Range Value | Numeric | A number representing the lower range value for the custom output range. | This field appears on the datasheet as a text box labeled Low, and is grouped with the following other fields in the Custom Output Details subsection:
|
Custom Output Range UOM | Character | The units of measure for the custom output range. | This field appears on the datasheet as a list labeled UOM, and is grouped with the following other fields in the Custom Output Details subsection:
If the Calibrator Type field contains the value Druck DPI620 (Genii) or Druck DPI61x, then this list is filtered by the value that you select in the Output Type field. This field is enabled and required only when the Custom Input Values check box is selected. This field appears as a list that is populated by the MI_CALIBRATION_IO_TYPES System Code Table. |
Custom Output Upper Range Value | Numeric | A number representing the upper range value for the custom output range. | This field appears on the datasheet as a text box labeled High, and is grouped with the following other fields in the Custom Output Details subsection:
|
Custom Output Values | Boolean | Indicates whether you will enter custom output values for the calibration. |
This field is enabled only when the value stored in the Calibration Type field is FLUKE 74x. When you select the Custom Output Values check box:
|
Engineering Units Error Limit | Numeric | A number representing the maximum amount of error in engineering units that is allowed before a calibration event is considered failed. |
The state of this field is dependent upon the state of other fields. Specifically, if the:
...where: You can modify the default value if required. This field is required. In case of a discrete template, the value stored in this field is the value that will be sent to the device. If you modify this value, then the value in the Max Error Limit (PCT) field will be updated automatically. In case of an analog template, the value stored in this field is converted into Equivalent Max Error Limit and sent to Calibrator. |
Input Damping Setting | Character | Indicates whether this setting should be on or off. When this field is set to On, the calibrator utilizes a secondary setting of damping time. This is applicable only to automated calibrations, and provides a delay between step changes that are applied to the device being calibrated. | This field appears as a list, and contains the following options:
This field appears as a list that is populated by the MI_DAMPING_TYPE System Code Table. |
Input Min Max Mode | Character | Indicates whether this setting should be on or off. When this field is set to On, the calibrator will store the Min and Max output values of the device being calibrated. This is applicable only to automated calibrations. | This field appears as a list, and contains the following options:
|
Input Type | Character | The input type for the analog calibration. |
This field appears as a list that is populated by the MI_CALIBRATION_IO_TYPES System Code Table. This field is required. The options that appear in the list depend on the value stored in the Calibration Type field. If the value in the Calibration Type field is Druck DPI620 (Genii), then you can choose from the following options:
If the value in the Calibration Type field is Druck DPI61x, then you can choose from the following options:
If the value in the Calibration Type field is FLUKE 74x, then you can choose from the following options:
If the value in the Calibration Type field is Analog-Manual, then you can choose from the following options:
Only pressure input values can be used with automated calibrations. |
Linear TC LRV | Numeric | A number representing the lower value on the linear thermocouple range. |
This field is enabled only when the TC Linear check box is selected. This field is populated automatically with values from the following fields, based on the value that exists in the Output Type field and the Input Type field:
|
Linear TC URV | Numeric | A number representing upper value on the linear thermocouple range. |
This field is enabled only when the TC Linear check box is selected. This field is populated with values from the following fields based on the value that exists in the Output Type field:
|
Loop Power | Character | A value that indicates the source of the loop power. |
If the value in the Calibration Type field is FLUKE 74x, then this field contains the following values:
If the value in the Calibration Type field is Druck DPI620 (Genii) or Druck DPI61x, then this field contains the following values:
If the value stored in the Calibration Type field is Analog-Manual, then this field is disabled. This field appears as a list that is populated by the MI_POWER_SOURCE System Code Table. |
Manual Entered Input Values | Boolean | Indicates whether you will manually enter the input value into the device during the automated calibration. |
This check box is cleared by default. Selecting this check box indicates that you will manually enter the input value into the calibrator during automated calibration. The state of this field is dependent upon the state of other fields. Specifically, this check box is:
|
Manual Entered Output Values | Boolean | Indicates whether you will manually enter the output value into the device during the automated calibration. |
This check box is cleared by default. Selecting this check box indicates that you will manually enter the output value into the calibrator during automated calibration. The state of this field is dependent upon the state of other fields. Specifically, this check box is:
|
Manufacturer | Character | The manufacturer of the Equipment that is linked to the Calibration Template. | This field is disabled and populated with the value stored in the Manufacturer field in the Equipment that is linked to the Calibration Template. If you have accessed the template from the library, then this field is disabled and blank. |
Max Error Limit | Numeric | A number representing the maximum amount of error in percent that is allowed before a calibration event is considered failed. |
This field is populated with the value 3 by default, as specified in the Analog Error Limit field in the Calibration Setup Defaults record. You can modify this value if needed. This value is used in the Calibration record to calculate whether a calibration event has failed or passed. |
Model Number | Character | The model number of the Equipment that is linked to the Calibration Template. | This field is disabled and populated with the value stored in the Model Number field in the Equipment that is linked to the Calibration Template. If you have accessed the template from the library, then this field is disabled and blank. |
Output Damping Setting | Character |
When this field is set to On, it indicates that the device utilizes a secondary setting of damping time. This provides a delay for the output of a device to stabilize after a step change that is applied to the input. This is applicable only to automated calibration. |
This field appears as a list, and contains the following options:
This field appears as a list that is populated by the MI_DAMPING_TYPE System Code Table. |
Output Type | Character | The output type for the analog calibration. |
This field is required. This field appears as a list that is populated by the MI_CALIBRATION_IO_TYPES System Code Table. The options that appear in the list depend on the value stored in the Calibration Type field. If the value in the Calibration Type field is Druck DPI620 (Genii), then you can choose from the following options:
If the value in the Calibration Type field is Druck DPI61x, then you can choose from the following options:
If the value in the Calibration Type field is FLUKE 74x, then you can choose from the following options:
If the value in the Calibration Type field is Analog-Manual, then you can choose from the following options:
|
Performs Square Root | Character | Indicates whether or not a square root calculation will be performed on the values in the Input Measure AF and Input Measure AL fields. |
This field is disabled or enabled based on the state of other fields on the datasheet:
This field appears as a list that is populated by the MI_YES_NO System Code Table. |
Primary Input LRV | Numeric | A number representing the lower range value for the primary input range. |
This field is grouped with the following fields in the Primary Input Details section:
The value stored in the Primary Input LRV field combined with the value stored in the Primary Input URV field define the primary input range for the calibration. This field is required. |
Primary Input Range Units | Character | The units of measure for the primary input. |
This field is grouped with the following other fields in the Primary Input Details section:
This list contains a list of UOMs that is filtered based on the value in the Input Type field and the Calibration Type field. This means that only the UOM values that are relevant for that input type and calibration type will appear in the list. After you select a value in this list, the GE Digital APM system checks to see if the UOM is compatible with the device. If the selected value is not compatible, then an error message will appear, indicating the problem. |
Primary Input URV | Numeric | A number representing the upper range value for the primary input range. |
This field is grouped with the following other fields in the Primary Input Details section:
The value stored in the Primary Input URV field combined with the value stored in the Primary Input LRV field define the primary input range for the calibration. This field is required. |
Primary Output LRV | Numeric | A number representing the lower range value for the primary output range. |
This field is grouped with the following other fields in the Primary Output Details section:
The value stored in the Primary Output LRV field combined with the value stored in the Primary Output URV field define the primary output range for the calibration. This field is required. |
Primary Output Range Units | Character | The units of measure for the primary input. |
This field is grouped with the following fields in the Primary Output Details section:
This list contains a list of UOMs that is filtered based on the value in the Output Type field and the Calibration Type field. This means that only the UOM values that are relevant for that input type and calibration type will appear in the list. After you select a value in this list, the GE Digital APM system checks to see if the UOM is compatible with the device. If the selected value is not compatible, then an error message will appear, indicating the problem. If the value in the Calibration Type field is Druck DPI620 (Genii) or Druck DPI61x, then this list is populated by the CALIBRATION_DRUCK_UOM_LIST System Code Table. This field appears as a list that is populated by the MI_CALIBRATION_IO_TYPES System Code Table. |
Primary Output URV | Numeric | A number representing the upper range value for the primary output range. |
This field is grouped with the following fields in the Primary Output Details section:
The value stored in the Primary Output URV field combined with the value stored in the Primary Output LRV field define the primary output range for the calibration. This field is required. |
Refresh Equipment Data | Boolean | Indicates whether or not information in the Equipment that is linked to the Calibration Template has been updated. | This field does not appear on the datasheet by default. This field is used by the GE Digital APM system, and should not be modified. |
RTD Wiring Configuration | Character | The RTD wiring configuration associated with the calibration. |
This field is enabled if:
If the value stored in the Calibration Type field is FLUKE 74x, then the RTD Wiring Configuration list includes the following additional options:
|
Serial Number | Character | The serial number of the Equipment that is linked to the Calibration Template. |
This field is disabled and populated with the value stored in the Serial Number field in the Equipment that is linked to the Calibration Template. If you have accessed the template from the library, then this field is disabled and blank. |
Tag Description | Character | The description of the piece of equipment that is linked to the Calibration Template. | This field is disabled and populated with the value stored in the Equipment Short Description field in the Equipment that is linked to the Calibration Template. If you have accessed the template from the library, then this field is disabled and blank. |
Tag Name | Character | The ID of the Equipment that is linked to the Calibration Template. This is the Equipment Technical Number of the Equipment. | This field is disabled and populated with the value in the Equipment field in the linked Equipment record. If you have accessed the template from the library, then this field is disabled and blank. |
TC Linear | Boolean | Indicates whether you want to provide a value in the Linear TC LRV and Linear TC URV fields. | This check box is cleared by default, and enabled only if the value in the Calibration Type field is FLUKE 74x and the Temperature Element Type field contains a Thermocouple value. |
Temperature Element Type | Character | The type of temperature element used for the calibration. |
The Temperature Element Type field is enabled and required only if the value in the Calibration Type field is not Analog-Manual and if the Input Type or Output Type fields contain the value Temperature. This field appears as a list that is populated by the MI_SENSOR_TYPE System Code Table. The temperature element types that are listed depend on the value stored in the Calibration Type field. If the value in the Calibration Type field is Druck DPI620 (Genii) or Druck DPI620 (Genii), then the following Resistance Temperature Detectors (RTD) and Thermocouples (TC) are supported:
If the value in the Calibration Type field is FLUKE 74X, then the following RTDs and TCs are supported:
If using a GE Druck calibrator, when you select None, a validation message appears, specifying that it is not a valid value. |
Template ID | Character | The ID of the Calibration Template. |
This field is required and must be unique. |
Template State | Character | The state of the Calibration Template. |
This field contains the value Development by default. This field contains the following values:
|
Copyright © 2018 General Electric Company. All rights reserved.