Calibration Strategy Records

Calibration Strategy records store information about the fields that are defined in the Calibration Strategy family in the baseline GE Digital APM database. This topic provides an alphabetical list and description of the fields that exist for the Calibration Strategy family and appear on the Calibration Strategy datasheet. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.

This family is not enabled for site filtering, which means that records in this family can be accessed by any user with the appropriate license and family privileges. See the Site Filtering section of the documentation for more information.

Field

Data Type

Description

Behavior and Usage

Down Count Numeric The number of records in the Down value range of the test point for a calibration strategy.

You can enter a value manually.

For GE Druck documenting process calibrators, the sum of the value in the Down Count and Up Count fields should not exceed 21 test points.

This field is required only if the Template Type field contains at least one of the following:

  • Analog Calibration
  • Single Component Analyzer
  • WeightScale Calibration
Strategy ID Character The ID of the calibration strategy

You can enter a value manually. The value must be unique.

This field is required.

Strategy Name Character The name of the calibration strategy

You can enter a value manually.

This field is required.

Template Type Character The type of calibration template.

This field appears as a list and contains the following Calibration templates:

  • Analog Calibration
  • Discrete Calibration
  • Multi-Component Analyzer
  • Single Component Analyzer
  • WeightScale Calibration
  • Functional Test

This field is required.

Up Count Numeric The number of records in the Up value range of the test point for a calibration strategy.

You can enter a value manually.

For GE Druck documenting process calibrators, the sum of the value in the Down Count and Up Count fields should not exceed 21 test points.

This field is required only if the Template Type field contains at least one of the following:

  • Analog Calibration
  • Single Component Analyzer
  • WeightScale Calibration

Copyright © 2018 General Electric Company. All rights reserved.