Calibration Profile Template Defaults Records

Calibration Profile Template Defaults records store information about the fields that are defined in the Calibration Profile Template Defaults family in the baseline GE Digital APM database. This topic provides an alphabetical list and description of the fields that exist for the Calibration Profile Template Defaults family and appear on the Calibration Profile Template Defaults datasheet. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.

This family is not enabled for site filtering, which means that records in this family can be accessed by any user with the appropriate license and family privileges. See the Site Filtering section of the documentation for more information.

Field

Data Type

Description

Behavior and Usage

Calibration Mapping

Character

The type of mapping.

This field appears as a list and is filtered by the value that you select in the Template Type field.

This field is required.

Custom Entered Values Character

A value that indicates weather the Profile Template that uses this template default will contain custom entered values.

This field must contain one of the following values:

  • Only Input (INPUT)
  • Only Output (OUTPUT)
  • Both Input and Output (INPUT AND OUTPUT)
  • None (NONE)
Device Type Character The type of calibration device.

This field does not appear on the datasheet and is populated automatically.

Error Configuration Character A value indicating the error processing configuration for automated calibration.

This field is disabled and is populated automatically with the value that you select in the Manual Entered Values field, as per the following table:

Value in Manual Entered Values Value in Error Configuration
Only Input (INPUT) UEV Source
Only Output (OUTPUT) UEV Measure
Both Input and Output (INPUT AND OUTPUT) UEV Measure Source
None Normal
Input Characteristic Curve Character A value indicating the characteristics of the input signal to the instrument being calibrated.

This field appears as a list and contains the following values:

  • Linear
  • None

This field is required.

Input Type Character The input type of the calibration.

This list is populated by the MI_CALIBRATION_IO_TYPES System Code Table.

You can choose from the following Input Types values:

  • Pressure
  • Temperature
  • Other

This field is required.

Manual Entered Values Character The type of manual value entered into the device during automated calibration.

This field appears as a list and contains the following values:

  • Only Input (INPUT)
  • Only Output (OUTPUT)
  • Both Input and Output (INPUT AND OUTPUT)
  • None (NONE)

Depending on the selection, the Error Configuration field is populated automatically.

This field is required.

Output Characteristic Curve Character A value indicating the characteristics of the output signal to the instrument being calibrated.

This field appears as a list and contains the following values:

  • Linear
  • None

This field is required.

Output Range Numeric A value that is used to define measurement range setting of the calibrator.

A value of 10 will set the Voltage range to 10 in the calibrator and the value in the Output Range Locked field will have to be set to 1 to enable this function.

This field is required.

Output Range Locked Numeric A number that represents if the auto range function in the calibrator is turned off or on.

The valid input values are 0 or 1.

  • If the value is set to 0, the auto range function in the calibrator is turned off.
  • If the value is set to 1, the auto range function in the calibration is turned on.

This field is required.

Performs Square Root Character A value that indicates if a square root calculation will be performed on the values in the Input Measure AF and Input Measure AL fields.

The values in this field are populated by the MI_YES_NO System Code Table.

This field is enabled only if the following criteria is met:

  • You can select the value Yes (Y) only if the value in the Input Type field is Pressure or Flow.

  • When the value in the Calibration Strategy field is 2 Down or 2 Up then 2 Down, this field is disabled and displays the value No (N).

  • You can select the value Yes (Y) only if the value in the Manual Entered Values field is None (NONE).

This field is required.

Template Defaults ID Character A unique ID for the template defaults. This field does not appear on the datasheet and is auto calculated.
Template Type Character The type of device mapping.

This list contains the following Calibration Templates:

  • Analog Calibration
  • Discrete Calibration
  • Functional Test

Depending on the selection, the Calibration Mapping field is populated automatically.

Copyright © 2018 General Electric Company. All rights reserved.