Amplification Codes records store information about the fields in the Amplification Codes family that are used to populate the Amplification Code field in a Primary Event record. This topic provides an alphabetical list of the fields that exist for the Amplification Code family and describes how the fields will be used to populate the Amplification Code field in an Event record. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.
This family is not enabled for site filtering, which means that records in this family can be accessed by any user with the appropriate license and family privileges. See the Site Filtering section of the documentation for more information.
Field |
Data Type |
Description |
Behavior and Usage |
---|---|---|---|
Amplification Code |
Character |
Identifies the cause of an outage and is used to populate the Amplification Code field in the Event record. |
By default, this field is populated with the Amplification Codes included in the Amplification Codes family. You can use the GAA Data Loaders to import the latest Amplification Codes. This value is defined by NERC in the GADS DRI and CEA in the Generation Equipment Status ERIS. |
Description |
Character | Describes the type of Amplification Code. | You can enter a value manually. |
Event Type | Character | Indicates the type of event associated with the Amplification Code. | A baseline rules exists to populate this field from the GAA Event Types family. |
Regulatory Organization | Character | Identifies the council to which data will be reported. |
A baseline rule exists to populate this field with a list of the following values:
This field is required. |
Unit Type | Character | Identifies the type of unit associated with the Regulatory Organization. | A baseline rules exists to populate this field from the GAA Unit Types family. |
Copyright © 2018 General Electric Company. All rights reserved.