Add a Production Event Code

You can add a Production Event Code that is the child of an existing parent.

Steps

  1. Access the Codes workspace.
  2. In the Choose code box, select Production Event Codes.

    The list of Production Event Codes appears.

  3. To add a child Production Event Code to an existing parent, select the check box next to the parent, and then select .

    The Add Production Event Code window appears.

    PLA Add Production Event Code Window

  4. As needed, enter values in the available fields.
  5. Select .

    The Production Event Code is saved.

Copyright © 2018 General Electric Company. All rights reserved.