The Risk Matrix that appears in the Risk Assessment window allows you to make selections that are used in calculations to determine an overall risk rank value.
The values that you see in the Risk Matrix are determined by various records. The baseline GE Digital APM database contains a Risk Matrix that you can use when evaluating risk, but if you do not want to use the baseline values, an administrative user can customize the default Risk Matrix or create a new Risk Matrix.
Note: See the administrative user documentation for the Risk Matrix for details on the records that make up the baseline Risk Matrix.
The following image displays the Risk Matrix that is provided in the baseline database, where no risk values have yet been specified.
Each tab in the Risk Matrix represents an area that might be affected if risk were to be presented. The Safety, Environment, and Operations tab each contains its own matrix, which combines in a grid format probability factors with consequence factors. The Financial tab contains text boxes that serve the same purpose.
Depending on how you access the Risk Assessment window, the risk matrix will represent either mitigated or unmitigated risk:
When a risk value is selected, the number on the corresponding tab is updated to indicate the specified risk.
In addition, the cumulative values specified in the risk matrix are used in a calculation to determine the overall risk rank, which is displayed in either the Mitigated Risk Rank or Unmitigated Risk Rank section on the right side of the window.
Copyright © 2018 General Electric Company. All rights reserved.