Install the Studio

IMPORTANT: This step is required only if you have the APM Connect Studio license. If you are deploying APM Connect Base with a Basic or Plus License, skip this procedure and proceed to the next step in the APM Connect Base deployment workflow.

Steps

  1. On the machine on which you installed APM Connect, access the Talend Studio installation package.
  2. Open the file TalendStudioInstall.exe.

    The Setup-Talend Studio window opens.

  3. Select Next.

    The License Agreement screen appears.

  4. Read the entire license agreement, and then select one of the following options:

  5. Select Next.

    The Select Destination Location screen appears.

  6. Select Next.

    The Select Components screen appears.

  7. Select the Add Start Menu Entry box, and then select the Add Desktop Icon box.

  8. Select Next.

    The Select Start Menu Folder screen appears.

  9. Select Next.

    The Ready to Install screen appears.

  10. Select Install.

    The Installing screen appears, displaying an installation progress bar. Once the installation is complete, the Completing the Talend Studio Setup Wizard screen appears.

  11. Select Finish.

    The installation is complete, and Talend Studio desktop icon is available.

What's Next?

Copyright © 2018 General Electric Company. All rights reserved.