Install the Meridium Integration Services

IMPORTANT: This step is required only if you are deploying APM Connect on-premises. If you are deploying in APM Now, you can skip this procedure, and proceed to the next step in the APM Connect Base First-Time Deployment Workflow.

Depending on your system architecture, you can perform this procedure on the APM Connect server or the GE Digital APM server.

Steps

  1. On the server, access the GE Digital APM distribution package, and then navigate to the folder \\Setup\Meridium APM Server and Add-ons.
  2. Double-click the file Setup.exe.

    The Welcome screen appears.

  3. Select Next.

    The License Agreement screen appears.

  4. Read the License Agreement and, if you agree, select the I accept the terms of the license agreement check box. Then, select Next.

    The Select Installation Location screen appears.

  5. Select Next to accept the default location.

    The Select the features you want to install screen appears.

  6.  Select the Meridium Integration Services option.

    Note: While additional options are available for selection, these options are not meant to be installed on this server. These instructions assume that you want to install only Meridium Integration Services.

  7. Select Next.

    The Websites screen appears.

  8. Select Next.

    The Complete the Installation screen appears.

  9. Select Install.

    The Setup Status screen appears, displaying a progress bar. Once the installation is complete, the Installation is complete screen appears.

  10. Select Finish.

    The Meridium Integration Services installation is complete

What's Next?

Copyright © 2018 General Electric Company. All rights reserved.