Note: If you using SAP PI, then you can skip this procedure.
If you use (S)FTP to transfer files between SAP, APM Connect, and GE Digital APM, you must complete additional configuration in SAP. You must download a puTTY file and set up command names in SAP to use the puTTY file.
Steps
In SAP, run the transaction code SM69.
The External Operation System Commands screen appears.
Select .
The Create an External Command screen appears.
Select Save.
The puTTY file is on the SAP system, and the corresponding command names are set up.
What's Next?
Copyright © 2018 General Electric Company. All rights reserved.