Configure Context Parameters

For every job that is imported, certain context parameters in the APM Connect Administration Center must be configured. This topic describes how to configure the required context parameters, so that you can run the job.

Steps

  1. In the APM Connect Administration Center, in the Job Conductor workspace, select the Job for which you would like to set parameters.
  2. At the bottom of the Job Conductor workspace, select Context parameters.

    The Context parameters section appears.

  3. In the Context parameter column, scroll down to the context parameter you would like to configure.

  4. In the Custom value box, configure context parameters, and select the Active check boxes for the following:

    The context parameters are configured.

  5. Repeat steps 1-3 for every imported Job you will run.
  6. To configure the Master job to run, select the SAP_MASTER_INTERFACE Job.
  7. At the bottom of the Job Conductor workspace, select Context parameters.

    The Context parameters section appears, displaying the following parameters:

  8. For each extraction jobs you want to run, in the Custom value column enter true, and then select the Active check box.

  9. In the MASTER_CONFIG_FILE_DIRCustom value box, enter the directory where the context file(s) is stored.

  10. In the SYSTEM_TO_RUNCustom value box enter:

  11. Press Enter.

    The Jobs are configured to run.

What's Next?

Copyright © 2018 General Electric Company. All rights reserved.