Configure the APM Connect Administration Center for the Studio

IMPORTANT: This step is required only if you have the APM Connect Studio license. If you are deploying APM Connect Base with a Basic or Plus License, skip this procedure and proceed to the next step in the APM Connect Base deployment workflow.

Steps

  1. Open a web browser.

    Hint: APM Connect is most compatible with Google Chrome or Mozilla Firefox web browsers. It is not recommend using Internet Explorer to access the APM Connect Administration Center.

  2. Enter the following URL into your web browser: http://localhost:8080/apmconnect/.
  3. If prompted, log in to the APM Connect Administration Center.
  4. In the Menu pane, in the Settings section, select the Configuration tab.

    The Configuration pane appears.

  5. Select the CommandLine/primary (5 Parameters) group to expand the workspace.
  6. According to the information in the following table, enter the necessary parameters.

    Parameter Description Recommend or Default Value
    Host The IP address of the CommandLine. localhost
    Port The port number on which the CommandLine is queried. 8002
    Job generation folder The path to the folder where Jobs are generated. <root:>\APMConnect\Utilities\cmdline\generationCache
    User component path The path to the folder where user components are stored. <root:>\APMConnect\Utilities\cmdline\custom_components

    The default parameters are configured as shown in the following image.

What's Next?

Copyright © 2018 General Electric Company. All rights reserved.